Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Power-grip driver

Power-grip driver
Sales Price: 8.99 SGD
Review Rating: 4.70
10 Customer Reviews
5 star 8
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Engine maintenance
5
From Japan
On 2018-06-20 19:48:40
The thickness of the grip is just right, it is hard to slip and easy to handle.
This review is about item#2197614.
Car Repair
5
From Japan
On 2018-05-08 18:00:56
Screws with magnets are not lost. The future will not slip forever. Good grip
This review is about item#2197623.
General
5
From Japan
On 2018-03-17 00:16:51
I've been patronizing nearly 30 years while replacing. I'm preliminary or emergency, I like tools, so I buy various drivers, but I always prepare full set with good tip without using main. Those with stronger magnetic force are easier to add iron powder and iron sand to that extent, some people dislike drivers that are plated to the tip, but those who are plated are overwhelmingly hard to rust, and the surface is plated It is also resistant to wear and it lasts long. Especially if you work with outdoor work or a wet place, this is kore. In addition, although this grip is red transparent, plug lips that have similar colors such as overseas products pb and xcelite and other transparent lips smell funny and will melt with acetone and others It is also strong against chemicals, it does not smell strange. But even people who use pb and xcelite have colors as well. It is about yellow transparent and red transparent so that the colors are aligned except black. The bolster part to wrench is also long and easy to use, and penetrates. It is a classic style that you want sold forever. In the past, the character print was yellow, but now it is white. Accuracy of tip? It's Bessel! The only problem is whether the main reason not to use is that the grip is hard and somewhat thin, so use with a single wrench is weak torque. In the company's products, the mega-dora enters power and soft grip sucks in hands. In other companies' products, the penetrating rubber grip of the annex oval Shimasima is easy to put power, but no bolster. I also love snap-on but it's not suitable for jis plus, so it's not penetrating so it's only for overseas products. Although Megadora may be the strongest after all, oil dirt is conspicuous and troublesome cleaning. I will return to this with such a thing. It is iteration of this for 30 years, but if you choose only one without having more than one, this is one choice.
Machine maintenance
4
From Japan
On 2017-04-17 15:04:46
Even though it is the 4th size, the thickness of the axis is not much changed, and it is easy to rotate without turning the whole part of + with the feeling of turning in the center part of +. It can be relieved that at least 1 mm or 2 mm thick.
This review is about item#2197641.
Various things such as motorcycle maintenance
3
From Japan
On 2015-04-21 08:30:56
Products of a vessel that can be safe. Piercing with a bolster. I tried this product for the first purchase. Easy to use, but I noticed using screws for a while but the attractive magnetic force is weak. Even if you use a tool (?) To magnetize the screwdriver, the magnetic force weakens immediately, that is the only drawback.
This review is about item#02197623.
DIY and car maintenance
5
From Japan
On 2015-02-01 19:10:23
It is good to be able to use wrench with good price, strength and usability.
Car maintenance
5
From Japan
On 2015-02-01 19:07:05
It is very convenient because it can be wrenched when turning screws by all means when using it for maintenance of a hobby car and DIY etc.
This review is about item#02197632.
Maintenance work for business use
5
From Japan
On 2014-06-01 18:03:44
Tip magnet, you can use with a wrench, you can buy this always because it's easy to use because the grip is thick and easy to put in force. Bessel made is also a reason for purchase.
This review is about item#02197623.
Machine maintenance
5
From Japan
On 2011-12-11 01:14:09
Push the tip so that it does not escape to the fixed screw, and loosen when turning and turning it with the glasses wrench. Although I have been using it for over 15 years, I can buy the same things so I can use it with confidence. (It is not a good translation to break)
This review is about item#02197623.
Removal of automobile parts
5
From Japan
On 2007-11-08 11:42:57
I am using it because I am well-balanced with price, strength, usability.
This review is about item#02197614.
1
Customer Who Viewed This Item Also Viewed
Megadora common driver
Power-grip driver
Super Cushion Driver
Penetration driver
Bolt Clipper
Slit Driver
ESD screwdriver
Pillow cover
Power Grip driver (through)
Power Screwdriver, Penetration