Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of A 45 degree double end face ring spanner

A 45 degree double end face ring spanner
Sales Price: 14.99 SGD
Review Rating: 4.00
7 Customer Reviews
5 star 3
4 star 1
3 star 3
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Bolts that are difficult to remove in SUBANA can be used without danger if this glasses wrench
3
From Japan
On 2018-05-12 17:44:08
Because it was often slippery when using SUBANA, it is easy to use because it is a long-length wearing glasses wrench.
This review is about item#2182975.
Machine installation
5
From Japan
On 2017-11-27 23:30:31
It is very good glasses. Cospar also well and the quality is also the best.
This review is about item#2183036.
Machine assembly
3
From Japan
On 2014-03-16 13:19:35
It is cheaper than other domestic products. Usability is normal. I think whether it is better than imported goods. There is no particular complaint.
This review is about item#02182932.
Repair of large car etc
5
From Japan
On 2013-05-04 19:47:36
For many years glasses wrench has been loving the super tool. From 10 mm to 36 mm is still super easy to use.
This review is about item#02182932.
To replace this round of round
3
From Japan
On 2012-12-01 12:56:01
Hitachi and Ryobi were 10 mm for this tip saw mounting bolt at hand, while 13 mm for cheap products for DIY. Although we can prepare wrenches separately, if I try to find a combination of 10 mm and 13 mm for anything in any case, 13 mm is not surprisingly small, as I found out here by chance , I immediately bought it. I do not feel a little slippery, but usability is normal.
This review is about item#02182941.
Brake adjustment of large cars, etc.
5
From Japan
On 2012-05-17 21:19:29
The angle is just easy to use and it is very nice
This review is about item#02182984.
Honda Today's "drive face" and "clutch outer" nut removal.
4
From Japan
On 2012-03-30 16:42:41
It was 14 x 17 and it took as long as possible. After 5 cm longer it will be saved, but ... It was in a state that nut licked a little, but it was unstable but went off without problem. Compared to the brand name, it seems that it only takes a bit of the sweet (shallow) it takes, but I think that it does not matter if ordinary work is done. Since it does not twist to the extent that it can be seen visually even if it exerts a considerable load. Capacity seems no problem. I think that it is good as a balance between price and performance.
This review is about item#02182984.
1
Customer Who Viewed This Item Also Viewed
Combination wrench
Long both mouth closed wrench
45deg x6 deg Long Offset Wrench
LOF 45° x7° Offset Wrench
OF 45 degree Offset Wrench
Box End Wrench
Double Ended Glasses Wrench
Long Base type Depth Gauge 300mm Base 250mm
Box End Wrench
L-Shaped Hex Wrench
Glasses wrench
Box End Wrench