Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Weight Scale

Weight Scale
Sales Price: 119.99 SGD
Review Rating: 4.86
7 Customer Reviews
5 star 6
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Weighing of agricultural chemicals
5
From Japan
On 2017-09-04 12:44:03
It is perfect for weighing liquid fertilizers and agricultural chemicals because the display is large in units of g.
This review is about item#3327721.
Check weight of shipping items
5
From Japan
On 2016-07-13 16:27:44
It seems to be strong as it looks and easy to use
This review is about item#03327737.
Provisional measure of product
5
From Japan
On 2015-09-25 16:16:19
It is about 2000 yen cheaper than the SD-12 purchase home center. I will continue to purchase.
This review is about item#02010872.
Weigh livestock feed
5
From Japan
On 2015-02-11 20:10:42
The scale we used once was for 2 kg. It was good when the amount of 1 kg was up to 2 kg, but if it was more than that, it was quite troublesome to measure in 2 divided doses, so I was looking for it, I found it with Monotaro and thought that I bought it unintentionally , Results It was easy to use and it was very good.
This review is about item#02010915.
Weigh foodstuff ingredients before use
5
From Japan
On 2014-09-25 17:51:21
I purchased it because the one I was using earlier was broken. It was cheaper than buying at other sites or shops. After all it was safe if it was the same thing that we used to date so we could purchase without hesitation.
This review is about item#03327737.
For weighing raw materials and for weighing when sending samples
4
From Japan
On 2013-07-30 13:48:50
Since I believe that it is a manufacturer with a small balance error, I purchase up to 12k newly It was easy to use because the end of the plate was bent upward until 8k which I bought a long time ago · · · It seems that it became flattened, so I think that we will try ease of use from now.
This review is about item#02010872.
Weighing the product
5
From Japan
On 2012-08-25 10:29:54
We are using it for measuring weighing products, so we have used Yamato because it was useless unless we passed the tests. There is a difference between SD and SDX, and the scale itself can be as large as 30 K in ordinary size. (Instruments with lower measurement limits should have no difference.) Only when I inquired to the maker by e-mail, there are only memories that were immediately answered ^ ^; I forgot which is oversized, but with popular type notation 10,000 The following is normal size and oversize exceeds 10,000. Because it might be good for an oversized type if weighing in a rice bag size with 30K total, I think that it is better to purchase it taking into consideration the size of the upper board.
This review is about item#02010915.
1
Customer Who Viewed This Item Also Viewed
Weighing Scale
Analog Weighing Scale K-1
Weight Measure, with Huge Scale Pan
Small Analog Scale
Even Balance Automatic Scale
Weighing Scale
Weighing Scale
Standard Weighing Scale SDX
Scale Cover