Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of The pack twist drill for stainless steel

The pack twist drill for stainless steel
Sales Price: 18.99 SGD
Review Rating: 3.86
7 Customer Reviews
5 star 4
4 star 0
3 star 2
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Drilling operation of sus316 sus316L
3
From Japan
On 2017-07-16 07:02:39
Sus304 can be used with confidence. Cospa is nice. Sus 316L has poor blade holding. The defect of the blade leads to defective products, so if the cospa is good, I would like a good one to hold. Especially in products which are hardened by the plasma of thick material, the blade holding is particularly bad.
This review is about item#05803165.
Drilling of stainless steel
5
From Japan
On 2017-06-19 15:11:26
Although it was processing for ordinary steel and steel it was bad and it was good without replacing the stainless steel well with the hole well
This review is about item#5803147.
Drilling of stainless steel
5
From Japan
On 2016-08-15 02:59:32
Good straight ahead and may last longer than a drill of Haisu
This review is about item#05803147.
Drilling in stainless steel
1
From Japan
On 2015-10-20 15:44:32
Kobelco's drill that he loved for ten years can not be finished, I bought this one which was good for review. However, the sharpness became suspicious from the area where the third hole was opened, and in the fourth hole, the fifth hole, it became almost the same as Kobelco used for 10 years. Is it because it is manufactured abroad (made in Singapore)? It's the worst. I will not buy it anymore.
This review is about item#05803113.
private
3
From Japan
On 2014-05-26 13:10:35
I used it to drill a hole in a fairly solid metal (material unknown), but it was not as bad as I thought it was. I was not able to open easily and I made it 1 useless ... It might be a problem of workmanship
This review is about item#05803113.
Steel (stainless steel)
5
From Japan
On 2013-01-04 18:11:56
I am using it in good condition. We would like to sell 5 sets in all sizes as well.
This review is about item#05803113.
Reaming of pilot holes
5
From Japan
On 2012-12-12 22:17:15
We are satisfied with processing of difficult-to-cut materials etc. There was a recommendation of a tool shop with dealings, and I was processing difficult-to-cut materials (HRC ≒ 25 steel) with a cobalt drill made by Mitsubishi Materials, but I was in trouble because my teeth were inconspicuous. By using this drill, we could finish machining without problem. I feel that there is also rigidity because the blade length is shorter than the other company's drill and the shank part is long. There are also people who evaluate it as easy to break, but I think that there is no problem in the place I used it.
This review is about item#05803192.
1