Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on May/30 2:00-3:00 JPT.
All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Heavy Baggage Pack, Thick Polyethylene Bag

Heavy Baggage Pack, Thick Polyethylene Bag
Sales Price: 4.99 SGD
Review Rating: 4.80
5 Customer Reviews
5 star 4
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Used for disposal
5
From Japan
On 2017-09-30 20:13:38
It is a sturdy bag that is quite thicker than usual and does not open holes even with some rubbing.
This review is about item#6597385.
After relatives' tombs, they are used to transport a few bags taken out in double bags for each person.
5
From Japan
On 2017-02-26 22:07:33
Because the contents of packing is special, it was requested that never pierce or cut wound during transportation. I chose a thing with enough thickness.
This review is about item#6597385.
Creation of old dog water bed
5
From Japan
On 2015-08-06 00:10:34
It was a hot summer and the old dog (dog) was in summer batte, so I made a water bed. Since the thickness of the usual garbage bag is 0.03 mm, there was a concern about water leaks easily because there was a hole, so I bought this product with a thickness of 0.1 mm. There was a poor adhesion on the product and there was a part where the water leaked from the beginning, but after that it was okay, there was no puncture even if I filled a cup of water, but this time, seal the mouth of the bag I had a hard time. It was an amazingly thick plastic bag.
This review is about item#06597385.
I bought it as a bamboo powder to put in.
4
From Japan
On 2014-07-11 13:43:06
We have not purchased chippers making bamboo powder yet, so we purchased only one for the time to see how much thickness and size it is. I thought it was a bit too thick. I think that the size is also about 30 liters.
This review is about item#06597394.
Used bag for withdrawing astringent persimmons with dry ice
5
From Japan
On 2013-11-07 14:34:34
- It is packaged in bags one by one, easy to use · It is firmly thick ground, holes are difficult to open in bags, durable
This review is about item#06597394.
1
Customer Who Viewed This Item Also Viewed
Commercial Plastic Bag
For Special Thick Plastic Bags
ECONO PLUS BOX (Boxed Type)
Special Thick Plastic Bag
Business-Use Plastic Bag
For Special Thick Plastic Bags
Commercial Thick Plastic Bags
Yo-Poly Bag, 0.1mm Thick
150L translucent MAX
Plastic Bag
Plastic Bag
Plastic bag for dust wagon
Econo Plus Large Garbage Bag