Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Tools for Remooving The Spruy

Tools for Remooving The Spruy
Sales Price: 20.99 SGD
Review Rating: 4.44
9 Customer Reviews
5 star 6
4 star 2
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Extraction of the sprue
5
From Japan
On 2018-05-01 11:45:31
I bought a set together with fittings etc. to extract the sprue. I can use it without problems.
This review is about item#5495497.
Screw repair
5
From Japan
On 2017-07-02 15:24:17
It is saved because various parts can be bought in bulk.
This review is about item#5495506.
Used when motorcycle engine overhaul
5
From Japan
On 2017-06-28 09:01:54
I inserted the recoil in the part where the screw part of the old engine became useless, but it was saved because it was able to pull out when inserting failed.
This review is about item#5495506.
Modification of motorcycle parts
4
From Japan
On 2016-09-28 18:46:58
In some cases, there are times when it can not be withdrawn, but it is possible to extract it almost as desired
This review is about item#5495506.
Extract helisert of the cylinder head of the motorcycle
2
From Japan
On 2016-02-14 17:00:52
It is used to pull out the m6 helical insert buried in the 6 mm hole a little behind the 6.5 mm hole. I could not use it if I had a helical insert at the back of the tool shape. I could scrape and shape it and be able to pull out safely. Did you mistake the size?
This review is about item#05495506.
In prototype process
5
From Japan
On 2014-07-08 18:08:37
Until now, work efficiency was also improved, as it was not being used, work was done cleanly and beautifully.
This review is about item#05495497.
Rescue in case of failure of sprue
4
From Japan
On 2014-06-11 08:41:13
The full length is long when it is a blind hole. There is no problem with the through hole, but it is necessary to fill the tip as necessary. I think that there is no problem if it is at the worker level where this kind of work is required.
This review is about item#05495497.
Sampling when the insertion of the sprue failed
5
From Japan
On 2013-04-01 15:33:01
I usually ask professional, but I do it myself when there is a missing etc., but I am unskilled because I am not so skilled, sometimes fail. It is useful at that time.
This review is about item#05495497.
Used to extract a mistake sprint
5
From Japan
On 2012-04-19 09:55:27
In the case of a base material such as aluminum, it may end up deeply. If you knead it deeply, the tip will crack. In the case of a sprint which is inserted much more deeply, there is a need to adjust to the size.
This review is about item#05495497.
1
Customer Who Viewed This Item Also Viewed
Coil Insert
Sprew P Insertion Tool
Extractor
Recoil Packet
Spry S Type Insertion Tool
Inserted Coil Pulling Out Tool
Sprew Repair Kit
Tangless Inserts
Coil Inserting Tool
Inserted Coil Pulling Out Tool
Tongue Breaking Tool
Extraction Tool
Sampling tool
1S2076S7A