Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Floodlight

Floodlight
Sales Price: -
Review Rating: 4.00
8 Customer Reviews
5 star 4
4 star 1
3 star 2
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Field lighting
3
From Japan
On 2016-02-25 21:04:03
Easy to use as the code is short
This review is about item#07087884.
Inside an incinerator
4
From Japan
On 2015-07-20 15:27:29
With cable 5 m, it is very convenient not to use the extension cable when installing in a high position. However, the ease of use of the mounting bracket breaks off immediately.
This review is about item#07087893.
Lighting fixtures at outdoor events
5
From Japan
On 2014-07-28 22:01:19
I used it at a company event beer garden. Holding on company premises. Clamp attached to the edge of the roof. Brightness is also satisfying at 500 W. Since there is not much price difference between 300 W and 500 W, it was 500 W. The price is about the same price even at other online shops, so Monotaro seems to be cheaper if you use coupons etc.
This review is about item#05763344.
On-site laboratory
3
From Japan
On 2014-05-19 13:33:59
Since prices are cheap, there is no particular need.
This review is about item#05763326.
As a machine maintenance light in the factory
2
From Japan
On 2014-01-21 13:09:13
It is somewhat dark. I thought it was even brighter.
This review is about item#07087893.
Used when working outdoors at night
5
From Japan
On 2013-10-02 13:59:24
Brightness was also good and night work was able to be done accurately ♪ I think that I would like to buy cheap again the price.
This review is about item#07087893.
For experimental irradiation of LED
5
From Japan
On 2013-06-15 13:21:56
It was necessary to extend, but there is no problem for the lighting test
This review is about item#07087875.
Add workplace lighting
5
From Japan
On 2010-04-30 12:31:09
Why is the light bulb sold separately for this low price? I was worried but I was with it. The brightness is satisfied. This length was enough because cables are also fixed completely by indoor wiring.
This review is about item#05763335.
1