Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Teddy bar

Teddy bar
Sales Price: 9.99 SGD
Review Rating: 4.60
5 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Deburring of the refrigerant pipe
5
From Japan
On 2017-03-01 19:49:02
It is small and it does not get in the way of sharpness.
This review is about item#6738103.
Deburring at the time of piping cutting
5
From Japan
On 2014-03-08 10:46:45
It is easy to use. I also have solid building.
This review is about item#06738103.
Hobby Craft
4
From Japan
On 2013-10-19 09:48:21
Previously, I used HOZAN or something, but there were times when the hands were thick and narrow place, there was a case where hands could not be used, but in this size the range of usable was expanded. Because it is a hard material, it seems to be strong. The sharpness is normal, but the size that can be used in a place narrower than the sharpness is important. There are several kinds of similar things, but this is the first time, this time it will be the second one. I do not feel bulky in my chest pocket and I think I can have several.
This review is about item#06738103.
Deburring of metal
5
From Japan
On 2012-04-23 22:10:52
I want cheap replacement blade for stainless steel
This review is about item#06738103.
Used for deburring deburring of aluminum material
4
From Japan
On 2011-12-05 13:43:19
There is a mistake in the notation of the set contents. Rotating blade is not S10 (BS1010) but N1 (BT1010) is the correct answer. I bought a replacement blade but I can not install it so I checked it with MonotaRO. We will correct for other purchasers.
This review is about item#06738103.
1
Customer Who Viewed This Item Also Viewed
Rotating blade
Noga bar 3
Super bar
Rotating blades
Blade B
Rapid bar
Rotating blades
SN holder
Unit UB1
Deburring Tool SHAVIV
Deburring Tool
Unit UB2
Unit UB 2000
Plastic edge offset