Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Test Indicators, Lever-Type Dial Indicator TI

Test Indicators, Lever-Type Dial Indicator TI
Sales Price: -
Review Rating: 4.70
10 Customer Reviews
5 star 8
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
When measuring shaft shake
5
From Japan
On 2016-11-21 16:50:49
I am satisfied because it is reliable and convenient as it is a manufacturer.
This review is about item#1997082.
Parallel out of vice with desktop milling machine
5
From Japan
On 2016-11-06 12:56:06
It is attached to the magnet arm and used for parallel out of the vice of the desk-top mill. I used an ordinary dial gauge but it was very difficult, but it is easy if it is a leverage formula. It is safe because it is Mitutoyo, and I'm glad I bought it.
This review is about item#1997021.
Rotary table centering
5
From Japan
On 2016-11-03 00:39:03
As expected it is a feeling like Mitutoyo. This movement is also smooth and easy to use.
This review is about item#01997003.
engine
5
From Japan
On 2016-03-25 17:48:57
Good!
This review is about item#01997012.
Centering with a lathe, in a milling machine operation, face, centering etc.
5
From Japan
On 2016-01-31 17:43:47
I am a person who is experiencing mechanical work as a hobby and refrain from being a professional. Although it has a general-purpose dial gauge, it is a type that is not a "lever type", so there is a difficulty in the position to fix, always measuring takes time or the value is not accurate. Since this product is a "leopard", such restrictions are relaxed, the sensing lever is sensitive and sensitive to weak forces, so it follows the measurement accurately, making the measurement setup easier and more accurate, reproducibility It also rose. Also, since the tip of the cantilever is thin and small, even in situations where it is impossible to measure up to now, measurement has become possible. The visibility of the display is also good, I am satisfied. Since there are many line-ups of products, if you buy for the first time, you may be at a loss as to which one to choose, but when you watch scenes actually used on video sites etc., "It's a thing to use like this" It can be understood and it may be useful for product selection.
This review is about item#01997012.
In the measurement of the machining center
5
From Japan
On 2015-04-06 16:12:15
I use it in the measurement of the machining center. I am using it to measure flatness but it is stable to use. It is Mitutoyo from the memory as well because it is easy to see.
This review is about item#01997021.
In glass polishing test
4
From Japan
On 2014-09-09 14:18:16
It was easy to use.
This review is about item#01996994.
Adjustment of core and surface of rotating device
5
From Japan
On 2013-06-01 14:14:55
The size is large and easy to see.
This review is about item#01997003.
Circle check on lathe
3
From Japan
On 2013-03-22 09:32:32
Usability as usual. I bought a MonotaRO brand before, but it is because Mr. Mitutoyo is good as it is because the pin was lost soon.
This review is about item#01997046.
Measurement of workpiece and core.
5
From Japan
On 2010-11-02 21:18:32
It is even better if a stem of φ8 is also set.
This review is about item#01997012.
1