Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Square Thick Wide Silver 50cm, Magnet

Square Thick Wide Silver 50cm, Magnet
Sales Price: 28.99 SGD
Review Rating: 3.50
2 Customer Reviews
5 star 0
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
High place inspection work
From Japan
On 2016-11-30 12:59:49
In work in a cold district, since thick gloves are used, it is difficult to handle with a magnet.
This review is about item#39246794.
Used during measurement work in narrow places and factories.
From Japan
On 2015-07-24 18:24:09
Until now, the curved line with no magnet is used, it is thick, and the treatment is called violent, quite a force like bumping or bending works, the bending waviness The precision was unstable, but since this bend is thick, there is no bend and it is appreciative that it will be hard to damage even if dropped, this time plus it plus 2 magnets in the short side direction Because it is stuck, it is convenient, it is convenient to be attached to ferrous materials, even if it is not stored in unstable elevations or working bags one by one, sand iron may also be attached somewhat It is a nice idea because it is good to wipe, thank you. I will come in handy.
This review is about item#39246794.