Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Submersible Pump (sanitary sewage pump)

Submersible Pump (sanitary sewage pump)
Sales Price: 239.99 SGD
Review Rating: 4.36
11 Customer Reviews
5 star 7
4 star 3
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Drainage of underground water storage
5
From Japan
On 2017-11-03 15:49:51
With drainage capacity more than expected, I had been pumping up with a bucket before, but I am satisfied very much because I can work easily with purchasing this time.
This review is about item#6741287.
Fetching water from a well
5
From Japan
On 2017-10-17 23:28:08
Easily enter the pond from a low well with Shimizu's movement. Both cost and capacity are satisfied.
This review is about item#6741271.
For septic tank, sludge return pump
5
From Japan
On 2017-02-12 15:58:26
8 units purchased SX 150 in 24 hours intermittent with 24-hour timer tap The other company (Engineering · Ryobi · Kawamoto) was flooded from the base of the cabire without having it for six months, but the leakage out of the Terada Pump Sex is remarkably high Now other manufacturers can not think about it http://blogs.yahoo.co.jp/tokaiama/28507858.html
Wastewater treatment pump
4
From Japan
On 2015-10-09 22:24:28
It is easy to use with a feeling that the pumping capability is exactly good, and very efficient work is done very much.
This review is about item#06741287.
Drainage
1
From Japan
On 2015-07-15 20:28:58
There is a noise during use, so when disassembling according to the instructions, one of the countersunk screws fixing the pump feathers has fallen. I wore it as it was, and just in case to confirm the tightening of the remaining two screws, one was normal and the other was loose, so it was tightened again and returned to normal. It is obviously a mistake in the manufacturing process or inspection process. I hope improvement of the manufacturer! It is!
This review is about item#06741271.
Drainage of water accumulated in the side groove
4
From Japan
On 2013-10-21 09:44:36
We did not use it for the drainage of the water that accumulated in the deep side groove. It was able to drain out considerably strongly. Since there is no switch, it is caution as it can be flooded with drainage if you do not properly prepare containers to be transferred. The last accumulated water will remain about 3 cm, but this was the best as we could improve drainage.
This review is about item#06741271.
Sprinkled on trees and flowers in the garden
5
From Japan
On 2013-04-22 15:03:40
Until now, I have pumped it by hand and sprayed it, but because it became available for spraying with a sewage pump, it can be sprayed on the trees that I could not spray until now, it is great saving. I should have bought it faster. It is light, easy to handle, and the difficulty of watering every morning and evening turned into pleasure.
This review is about item#06741271.
Sewage treatment
5
From Japan
On 2013-03-14 08:25:19
I am more satisfied with the power than I thought.
This review is about item#06741287.
In the excavation hole at the spring water
5
From Japan
On 2012-11-12 22:12:45
I use it in sand mud. It is lighter and lifts with one hand. But there is ability and usability is the best. This is enough if it is not a lot of drainage.
This review is about item#06741287.
Transfer of residual water in aquarium
4
From Japan
On 2011-10-23 13:17:07
It is suitable for work in a place where the diameter is small with a cylindrical pump and the dropping port of the pump is narrow.
Drainage sewage water supply
5
From Japan
On 2009-10-16 21:45:09
Although I have purchased 1 or 2 units per month, water quality mixed with wastewater (sand, mud), etc. but compared with pumps of other companies the reduction of the impeller is also late and will last long. I can recommend it.
This review is about item#06741271.
1
Customer Who Viewed This Item Also Viewed
Stainless Sickle
Submersible Pump Compact
Submersible Pump, Construction
Sludge Submersible Pump
Family Submersible Pump, Tsurumi Pump
General Dewatering Pump LB
Submersible Pump CSL
Sludge Submersible Pump, Light Resin
Family Pump
Wastewater Pump
Submersible Sewage Pump
Underwater Pump
Submersible Pump, Ponster