Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pressure Switch

Pressure Switch
Sales Price: 61.99 SGD
Review Rating: 4.86
14 Customer Reviews
5 star 13
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 14 of 14 Reviews
When compressor maintenance
5
From Japan
On 2017-10-17 14:34:48
It is a very easy-to-use item. Operation is smooth, installation is easy.
This review is about item#2105713.
Using nailing machine at construction site
5
From Japan
On 2016-07-21 20:45:55
Replacing the Max pressure switch is used without any problem.
This review is about item#02105722.
Exchange of air compressor pressure switch
5
From Japan
On 2016-07-10 20:55:41
I set the set pressure according to the scale. It was accurate at the same scale position as the indication value of the pressure gauge. The operation is good.
This review is about item#02105722.
Repair of old babicon
5
From Japan
On 2016-05-02 11:24:59
Before buying another person's review (below) - Stop when the set pressure comes down Stop from that pressure even a little descent There is no width between the start of watching - I was worried but actually no hindrances. I used it for replacing the pressure SW of the old Hitachi Babicon with good indicator of pressure set value.
This review is about item#02105713.
A piece of vacuum distillation.
5
From Japan
On 2016-03-10 15:01:43
Accuracy is still uncertain but good.
This review is about item#02105713.
Compressor power supply automation
5
From Japan
On 2015-10-13 20:32:43
Electricity saving, economical, because the motor has been running around until now because the power will be turned off automatically.
This review is about item#02105722.
Mounting on compressor
5
From Japan
On 2015-09-14 21:14:45
Once turned on the power automatically turned on and off with stable pressure and became power saving.
This review is about item#02105722.
For compressor pressure switch replacement
3
From Japan
On 2014-12-31 18:20:42
Stop when it reaches the set pressure Stop from that pressure even if it falls even slightly There is no width between the start Whether the width can be adjusted will be expensive This is enough if used only occasionally.
This review is about item#02105722.
Updated air compressor pressure six switch
5
From Japan
On 2014-10-28 20:39:01
It was as planned.
This review is about item#02105722.
For compressor starting and stopping
5
From Japan
On 2014-09-19 23:19:03
Start and stop Better if you can adjust the pressure difference. Others are satisfied.
This review is about item#02105722.
Replacement of defective parts
5
From Japan
On 2014-01-28 15:25:07
Compact and easy to replace.
This review is about item#02105731.
Control of air pressure
5
From Japan
On 2014-01-12 19:53:56
An arbitrary pressure setting is possible between 0.5 MPa and 2.0 MPa, which is easy to use. The contact output is always closed and always open, depending on the connection terminal. If the contact is connected to the electromagnetic switch, automatic operation becomes possible. The cover can also be detached with a single screw, so maintenance is easy.
This review is about item#02105731.
I used it as a compressor pressure SW
5
From Japan
On 2013-04-14 23:00:06
I wish there was a time lag between SW on and off
This review is about item#02105722.
Repair of air compressor
5
From Japan
On 2012-04-30 22:23:49
It works without problems
This review is about item#02105731.
1
Customer Who Viewed This Item Also Viewed
Pressure Switch
Flow Switch
Pressure Switch
Pressure Switch
pressure switch
pressure switch
pressure switch
Adapter