Buy more than* S$200* and get FREE SHIPPING
Our website will be under scheduled maintenance from 14th October 2017 11:00PM to 15th October 2017 1:00AM (Singapore Standard Time).

Customer Reviews of PRESTO Straight Type

PRESTO Straight Type
Sales Price: 28.68 SGD
Review Rating: 4.62
32 Customer Reviews
5 star 26
4 star 3
3 star 1
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 20 of 32 Reviews
Soldering and removing parts from the base
5
From Japan
On 2017-02-12 08:36:07
It is very convenient to be able to adjust the amount of heat immediately. Those with large heat dissipation surfaces, thick cables, etc. that could not be welded until now have become possible. Also, the included heat-resisting cap can be safely turned on very quickly. It is likely to be favorite for a long time.
This review is about item#02210521.
It is used for soldering repair of electric parts, wiring connection, etc.
5
From Japan
On 2016-12-27 16:18:00
Temperature rise time to use (possible) is short, heat quantity is sufficient, work is easy, easy to use.
This review is about item#2210521.
Vehicle wiring repair work
5
From Japan
On 2016-11-09 10:35:07
As for this product, the rising tip temperature was also early and the feeling of use was good.
This review is about item#2210521.
Field soldering
5
From Japan
On 2016-05-06 10:53:17
It is a standard product that I have been using for 30 years. I lost it this time, so I placed an order. Since there is no breakdown for a long time and there is no temperature setting, it is not troublesome and warms up quickly, so it is a wonderful item that is extremely easy to use.
This review is about item#02210521.
Soldering of fine electronic parts, thick copper wire, wire etc.
5
From Japan
On 2016-03-31 18:01:51
The soldering iron tip is strong against heat, and it is also suitable for soldering fine parts while it is a high power output, improving work efficiency.
This review is about item#02210521.
Soldering work etc.
5
From Japan
On 2016-03-20 22:24:08
It is convenient to be able to adjust the temperature at hand. It is more convenient if it becomes cordless.
This review is about item#02210521.
20 W - 130 W
1
From Japan
On 2016-02-23 11:02:30
I bought it thought that it can be varied, but only at the time of launching and pressing the button 130W and after 20W will not be used
This review is about item#02210521.
Repair of precision board
5
From Japan
On 2015-12-27 10:51:36
It is small and easy to use. The temperature can be switched by a button type.
This review is about item#02210521.
Soldering operation outdoors
5
From Japan
On 2015-12-22 14:45:05
Power switching is grateful. Soldering outdoors is difficult in securing tip tip temperature, heat-up switch is effective.
This review is about item#02210521.
Required repair etc.
5
From Japan
On 2015-12-22 10:09:51
Since the thing which I used to date has been broken, I purchased it, but it's pretty easy to use.
This review is about item#02210521.
PC parts adhesion
5
From Japan
On 2015-12-09 15:29:55
There is no protrusion on the tip part, and the position of the Wattage Increase button is also good, and it will fit nicely in your hand.
This review is about item#02210521.
Used for maintenance of acoustic equipment, repair etc
5
From Japan
On 2015-11-09 11:39:09
It gets used temperature soon, it is perfect for me of irritation ('∀ `)
This review is about item#02210521.
For ordinary soldering work
5
From Japan
On 2015-10-11 15:09:28
The thing which used before was solder thinning, it is hard to use (oxidized and the tip of the tip can not come off), so purchase. Since it is almost the same specification, it can be used without problems. It is extremely appreciated that the tip cap was attached.
This review is about item#02210521.
Wiring and board soldering
4
From Japan
On 2015-09-12 17:49:41
Although it is satisfactory in terms of performance, it will be easier to use if the power cord is softer. Also, as the button switch for boost is placed on the bottom side, putting the iron on the flat surface will keep the switch on and it is good to have a guide with the same height as the button on both sides of the button switch I will.
This review is about item#02210521.
Toy repair, electronic work
5
From Japan
On 2015-07-17 15:06:53
1 Iron tip 0.25 mm was attached, but an ellipse of 0.5 mm or 2 mm was good. 2 The code is hard and the degree of freedom is sacrificed a little. 3 Booster is truly comfortable. 4 Cap is good, it is effective for protection of the trowel. 5 If you want greed, boost buttons will come up when you grab and stabilize. Satisfied overall.
This review is about item#02210521.
Soldering of wiring
5
From Japan
On 2015-07-06 19:40:02
Although I bought it because the price was cheap, heating is quicker than I thought it is very easy to use! The tip is also thin, so it is optimal for wiring solder.
This review is about item#02210521.
Printed circuit board assembly
5
From Japan
On 2014-12-03 08:43:07
It is a replacement as the iron tip of the same product I bought about five years ago has become short. I also bought the same thing because it was easy to use although I replaced the previous tip twice. This time I can relieve for a while because I bought 5 pieces of main part and iron tip, 5 pieces of protective pipe. It is convenient because it can make it in time for soldering a cable of about 5 φ from a flat IC (1.27 pitch) because this one is in time.
This review is about item#02210521.
It is a reliable manufacturer. Used for bonding copper wire
5
From Japan
On 2014-11-04 13:59:43
Procurement of parts is readily available so we continue to use Hikari. First of all, I am relieved for products and will continue to use it. Thank you Mr. Shirakawa ...
This review is about item#02210521.
Soldering of universal board, connector
4
From Japan
On 2014-07-09 08:50:35
Although it is heavily used for soldering the connector, if the small tip is attached, the tip is sharp and melting of the solder is bad, so we replaced the small tip with a round shape. When using the UEW line, since the output is raised with only one button, it is convenient to melt the film easily.
This review is about item#02210521.
Soldering of electronic components
4
From Japan
On 2014-02-18 00:53:21
I used the same thing as before (good made), I wanted another one to be spare and easy to use but I was giving up because it was not sold any more, I bought this by watching this white light PRESTO. Usability is as easy to use as before. (When you want to solder in a hurry, you can solder it as soon as you press the button, so one item you can not release) The good point is put in the tool box before it is completely cooled because it has a cap.
This review is about item#02210521.
1 2