Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Repeat Tie

Repeat Tie
Sales Price: 8.99 SGD
Review Rating: 4.40
10 Customer Reviews
5 star 7
4 star 2
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Temporary fixation of tools, cord, bond of hose.
5
From Japan
On 2018-05-09 18:30:37
Because it used it for the product from before, it is a safe maker. This time, we misunderstood the length and ordered a little too short, so reorder intend to do something.
This review is about item#6682015.
Motorcycle repair
5
From Japan
On 2018-03-08 15:52:02
Temporarily fix it, or use it when wrapping the electric cord. It is convenient because it can be removed with one touch and reused.
This review is about item#6542015.
For harness fixing of motorcycle
5
From Japan
On 2018-01-30 19:22:18
I used it to fix the electric system running along the frame of the bike. Nylon tie of the type which was originally releasable was used, but exchange was carried out one way as hardening due to secular change was severe.
This review is about item#6542015.
For binding or temporary fixing
5
From Japan
On 2017-08-29 21:02:07
It is economical and convenient because it can be reused repeatedly for various uses. Even if it fails it is handy because it just pushes it off with a nail. I would be more pleased if things like a guide are attached to the remaining part after binding.
This review is about item#6682024.
Piping of watering equipment
5
From Japan
On 2016-09-29 19:36:25
It is convenient because you can repeat even if you stop differently. I am satisfied with the price as well.
This review is about item#6542042.
Wiring arrangement
4
From Japan
On 2016-04-13 17:40:48
There is not a hard feeling in particular, it is easy to use.
This review is about item#06542015.
To bundle wires
4
From Japan
On 2016-01-31 17:14:29
It is convenient to be able to reuse although it is used when it is necessary to remove bundled wiring. I think that it is a matter of material, but it is hard to use when wrapping around wiring for hard hard. I think that it is the hardness required for the lock mechanism, but unlocking is hard and it is difficult to release it so I think that it is a little soft and easy to use.
This review is about item#06681981.
Binding work
5
From Japan
On 2016-01-27 16:16:06
It is slightly harder than the type without weather resistance.
This review is about item#06542042.
Bundle of wiring cords
5
From Japan
On 2013-10-16 13:50:57
When we re-extend etc. we return the unity and use it conveniently as necessary to reassociate.
This review is about item#06681981.
Used to close plastic bag
1
From Japan
On 2012-07-13 15:06:26
There are defective products at frequencies of 1 to 2 in 20 bottles, which is troubling. Please improve.
This review is about item#06542015.
1
Customer Who Viewed This Item Also Viewed
Black Cable Tie
Wire Band With Lock
Repeat Tie
ECO insulation lock repeat type
Repeat Thai High temperature environment type
Tie wrap
Repeat Tie
  • Repeat Tie
  • HellermannTyton (former Tyton)
  • 14.99 SGD
Cable Tie
It made repeat Thailand polypropylene
Repeat Tie
Releasable Tie, Repeat Type
Cable Tie, Repeatable
Binding Band Repeat Type