Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Anti-Vibration Pad

Anti-Vibration Pad
Sales Price: -
Review Rating: 4.40
10 Customer Reviews
5 star 7
4 star 2
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Use of dust collector
5
From Japan
On 2016-01-31 10:41:49
I used it internally when creating a box to use a dust collector inside the classroom, did it have any effect? I am satisfied with my self.
This review is about item#11127557.
It laid it on the bottom of the drilling machine
5
From Japan
On 2015-04-30 09:39:20
There used to be vibrations and sounds before but when we laid a vibration isolating pad between the drilling machine and the table, we heard a motor sound, but both vibration and sound disappeared. I can work very comfortably. It was good to purchase. Thank you very much.
This review is about item#11127541.
Anti-vibration measure of washing machine
5
From Japan
On 2015-03-27 18:39:59
Because the vibration was severe when using the washing machine for a long drying mode, we installed this product. Although the vibration of the washing machine itself does not change, vibration transmission to the floor has decreased.
This review is about item#11127523.
Set between the legs and the floor of a large machine
5
From Japan
On 2015-03-20 14:35:16
There was no dramatic change, but it was pretty satisfying.
This review is about item#11127557.
Anti-vibration countermeasures for capacitors and transformers
5
From Japan
On 2015-01-23 13:20:42
I do not know because it will be used at the end of this week, but I have judged that there is no problem because there is a track record of construction similarly
This review is about item#11127557.
Reduction of vibration of air-conditioner outdoor unit, measures against vibration noise of personal computer
5
From Japan
On 2014-07-24 14:04:58
With the thick rubber, because it was worrisome about vibrating sound of PC (due to two HDDs placed on the main body and because the housing is distorted due to aging), it is getting worse when laying the anti-vibration pad The vibration sound also stopped, the rest was laid in the air-conditioner outdoor machine which was the original purchase purpose, even if it is used in the room, there is no smell peculiar to rubber, if it is no problem with the manufacturer, it may be available for audio speakers I have not confirmed the color transfer, so I do not understand it
This review is about item#03394571.
Two-layer washing machine
1
From Japan
On 2014-06-26 13:30:47
As the washing machine moves during dehydration I tried laying it underneath but the mat is soft So it's jerky shaking and moving when dehydrating (+ o +) Do you try to lay it under a compressor
This review is about item#03394571.
Vibration isolation of vibration sieve
4
From Japan
On 2013-05-15 14:28:35
Existing rubber was exchanged due to hanging, vibration to the floor disappeared due to the exchanged effect, vibrations of the sieve became large, even if the vibration slowly made sufficient sieve function appeared.
This review is about item#03394571.
Vibration countermeasure of air compressor
4
From Japan
On 2012-09-01 23:28:28
Since the air compressor is noisy, as one measure, I tried laying this pad down. I think that the vibration was suppressed as it was.
This review is about item#11127584.
I use it as a countermeasure against vibration of desk milling machine.
5
From Japan
On 2008-07-29 00:23:28
Compared to before use, vibration and chatter are suppressed.
This review is about item#03394571.
1
Customer Who Viewed This Item Also Viewed
Antivibration Rubber
Vibration Pad, Chloroprene Rubber,
Anti-Vibration Pad
Anti-Vibration Pad
STEP CLAMPS
Anti-Vibration Pad
Anti-Vibration Pad IP-Type
Anti-Vibration Rubber