Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Handy Sj Digital Measure

Handy Sj Digital Measure
Sales Price: -
Review Rating: 4.50
4 Customer Reviews
5 star 2
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Measure load during mast setup of competition yacht
5
From Japan
On 2017-08-07 14:46:20
It is easy to set 0 points and it fits the purpose of use. A spring scale may also be used, It is suitable for load measurement within a specific distance.
This review is about item#6859246.
I bought it for the purpose of measuring the operation load of the side door pulling door.
4
From Japan
On 2015-12-24 08:34:56
Thank you for shipping urgently. I got it in time. As a demand, I think that it would be nice if we had a function to hold the stable load automatically. The target product is a structure that pushes the hold button during measurement. I would like to continue purchasing if there is a machine in the future. Thank you very much.
This review is about item#06859246.
Weigh the merchandise on the go
5
From Japan
On 2014-07-30 20:56:20
The size of the handle is also exactly good, compact, it is easy to use because it is easy to carry because it is not bulky. Since notes on water wetting are not written, we are worried about the trouble due to digital.
This review is about item#06859246.
Weighing at the time of going out
4
From Japan
On 2012-08-30 16:21:30
Although it is a good product to the extent expected, it is also dissatisfied. [Good point] Battery consumption during off is small (about the minimum measured value of 0.1 μA) 3 to 4 mA when on. In Japan it is difficult to obtain Inch tape measure is also convenient. Because the resolution was suppressed to 50 g, the display is stable and it is very easy to use. [Defect] It is convenient that there is a handle, but it is better if it can be pushed in and rotated to accommodate it in the main body. Accuracy is not stated in the manual. If accuracy is not guaranteed, I would like to buy cheaper products. On the premise of stable display, we want a resolution of 10 g while maintaining a maximum of 50 kg (500 N). Handle · display · switch size should not be changed, the whole should be smaller. (The reason for not continuing to purchase is satisfied with this one)
This review is about item#06859246.
1
Customer Who Viewed This Item Also Viewed
Digital Force Gauge
Spring Scale
Digital Scales
20kg Spring Scale
Force Gauges
Automatic Manual Measurement Only
Hook Scale Mini
Set file 8 pcs round rough
Pipe Hand Scale