Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Geared Motor, GM-S Series, 0.4KW

Geared Motor, GM-S Series, 0.4KW
Sales Price: 289.99 SGD
Review Rating: 4.50
4 Customer Reviews
5 star 3
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
For driving the sieve (sieve)
5
From Japan
On 2017-01-07 17:41:00
It is used for driving the sieve fruit. Until now I was shaking the sieve by hand, but I used the link mechanism using the crank of the bicycle to drive the sieve. I use it in combination with the same Mitsubishi inverter, but I can use it quite well. I believe it has become an era when such products can be easily obtained at low cost and used.
This review is about item#6870272.
Motor change
5
From Japan
On 2015-11-23 15:17:21
Small noise is quiet, exhaust heat is also good. It was cheapest.
This review is about item#06870263.
Used as accessory for crusher plant crusher
3
From Japan
On 2013-11-14 13:11:02
Toshiba's motor was good, but I bought it because it was not there.
This review is about item#06870263.
As a drive for liquid pump
5
From Japan
On 2013-04-24 16:44:05
Horsepower uses mostly small objects, but there is no problem at all. The price is also cheaper than other manufacturers and there is no problem with size and weight. However, if you want to use grease, I will mainly use coupling, but there is nothing with hole diameter suitable for this motor, it is a problem that we have to arrange couplings and hole drilling to other companies by themselves .
This review is about item#06870245.
1
Customer Who Viewed This Item Also Viewed
Geared Motor, GM-S Series, 0.2KW
Geared Motors
Geared motor GM-S Series
Geared Motor, No-Brake
Geared motor GM-J2 series
Giyamotoru TA series (three-phase 200V)
Geared Motor 0.1KW
Geared motor GM-SP series (leg mounting)
Geared Motor, GM-S Series, 0.75KW