Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Magnetic Base

Magnetic Base
Sales Price: 65.99 SGD
Review Rating: 3.36
11 Customer Reviews
5 star 2
4 star 5
3 star 1
2 star 1
1 star 2
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Micrometer holder
4
From Japan
On 2017-12-09 18:45:34
Purchased a little narrower. I felt that the magnetic force was a little weak, so push four.
This review is about item#6897484.
Measurement of shaft runout of milling machine
2
From Japan
On 2017-05-01 15:15:06
It is good to be small, but weak holding power at adsorption, it moves. Also, since the holding force ON-OFF changeover switch of the magnet is too hard, the position moves when switching.
This review is about item#6897484.
Adjust shake of lathe work
5
From Japan
On 2015-12-28 16:20:05
I used a standard magnet base with a mini lathe so far, but alignment of the dial gauge was rather troublesome. Meanwhile, I found another Flexible Mini Magnet Base that I found another one that needed a magnet base for another use and bought it. To be honest, it seemed easier to use than the previous one, but I am surprised to use it, I am satisfied because I can set it with almost one action.
This review is about item#06897484.
Setting of machine tool workpiece
4
From Japan
On 2014-07-08 09:29:17
There is no problem in use, but the lock part differs from the photo What is different?
Main spindle core
4
From Japan
On 2013-03-12 18:08:16
I mentioned that the flexible part is loose with the previous review, but when tightening the middle lever, you can use the upper and lower flexible parts for tightening work without problems, I was disappointed. What principle? I guess.
This review is about item#06897484.
Gauge attached to core squares etc. of machine tools.
5
From Japan
On 2012-06-29 21:00:27
Since the arm is short-circuited, it is easy to measure with a small gauge marked with a small gauge in a narrow place.
This review is about item#06897484.
For support of dial gauge for centering inspection such as coupling
1
From Japan
On 2011-06-27 21:34:59
Since the fixation of the flexible part sweetly rotates 360 degrees and uses it, since the position of the tip is slightly displaced, the indication value of the dial gauge is not reliable and there is no value of the product ⇒ Again the made in China is cheap Can not trust? Is it useless if you choose prices and product introductory sentences? I think.
This review is about item#06897484.
Used as fixing jig for sinker
3
From Japan
On 2011-05-27 04:05:01
Although the product size is very satisfied, I am concerned about the weakness of fixing the magnetic force and the flexible. However, this size at other manufacturers is personally saved because the amount of money changes a little.
This review is about item#06897484.
Centering work
1
From Japan
On 2009-06-12 20:59:13
If you purchase it and start using it recently, the root is loose and I would like you to exchange it. The two previous products can be used without problems.
This review is about item#06897484.
Fan, main spindle of pump and used for adjustment
4
From Japan
On 2009-03-25 19:09:12
I think that it is good to be satisfied with the price, and improve the point of completely fixing the flexible part a little more.
This review is about item#06897484.
The core of the coupling
4
From Japan
On 2007-10-18 08:48:13
It can not be fixed unless it is tightened strongly. It can be locked with something like a small lever, even better.
This review is about item#06897484.
1