Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Stainless Steel Punched Sheet

Stainless Steel Punched Sheet
Sales Price: 20.99 SGD
Review Rating: 4.40
10 Customer Reviews
5 star 7
4 star 2
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Protection of clutch
4
From Japan
On 2018-03-14 20:31:47
When replacing plastic ones with this stainless steel, durability was improved. There is a border, so it is comfortable without getting caught.
This review is about item#7015942.
To the sound deadening material in the drum of the muffler of the automobile that melted down (round and fix it)
5
From Japan
On 2018-02-22 22:49:56
I bought and processed the aluminum punching board at the home center first, but it seemed to melt with heat anyway, so I changed to here. I am using it with confidence that it seems to be strong even for strength and enough for heat.
This review is about item#7015942.
For motorcycles
5
From Japan
On 2017-09-28 20:03:25
I wound up scratches on silencers of mufflers hidden. It is a predictable appearance. 0 040 04040 0404040 04040 04040 04040 04040 04040 04040 040 040 04040 04040 04040 04040 040 040 04040 04040 040 040 040 040 040 04040 040 0 040 040 040 0 040 0 04040 040 0 040 0 040 0 04040 040 0 0 0 0 0 0 0 0 0 0 0 0 0 040 0 Lol.
This review is about item#7015942.
Netting of ditch
5
From Japan
On 2017-01-13 15:49:06
I wanted something slightly thicker, but I got the strength and secured strength. I'd like more variations in size.
This review is about item#7015942.
Used for work
5
From Japan
On 2016-11-25 14:44:08
Goods are also firm, quick dispatch, courteous packing! There is no complaint arrangement. I will also use it.
This review is about item#7015942.
Lower cutter of laser cutter
1
From Japan
On 2016-11-09 07:14:01
This board has large distortion. If it is placed on a flat surface, the edge will float about 10 mm. I thought about using it on the lower plate of the laser cutter, but I can not use it very much. I heard that this product is such a thing when I contact support.
This review is about item#7015951.
Used as drying working plate
5
From Japan
On 2016-11-09 06:37:41
It is easy to process and can increase strength
This review is about item#07015951.
Used as Ikes' strainer
4
From Japan
On 2015-10-16 08:49:56
It is used by welding processing. Because it can not be welded if it is left unattended, it is good to be able to weld the end with this product.
This review is about item#07015942.
Foundation ventilation opening
5
From Japan
On 2015-08-22 16:20:33
I used it for the ventilation hole of the foundation, because it is too fine with the existing mesh, I exchanged for this punching, it is convenient because it can be installed and cleaned outdoors.
This review is about item#07015951.
For the HDD shelf board of the external storage device of the personal computer
5
From Japan
On 2014-06-15 21:05:19
Although it may be a wicked usage method, since HDD is weak against heat, we used it as a shelf board to make it ventilated. I am satisfied with my workmanship as I expected.
This review is about item#07015942.
1
Customer Who Viewed This Item Also Viewed
Aluminum Punching
Aluminum Mesh Netting
Punching Panel
Stainless steel crimp eyes Battoami
Punching board
PA type aluminum punching plate
Back net