Customer Reviews of LED magnetic flexible light
The reviews are automatic translation.
Showing 1 - 20 of 47 Reviews
Used when indoor lighting is not enough.

From Japan
On 2018-03-07 14:48:17
Both price and usability are satisfactory, but in other words there were things that required drivers for battery replacement and things that did not turn on for one year.
This review is about item#7063131.
Used for machine maintenance

From Japan
On 2018-01-19 23:26:23
Although it is compact and lightweight, the light is darker at the beginning, there is a flexible difference in the line, but it is sweet to fix the light.
This review is about item#7063131.
Confirmation of scribe mark of slide circular saw

From Japan
On 2018-01-19 15:54:04
The operability of the switch that fits the review is tolerable. I want a battery other than a button battery
This review is about item#7063131.
Used for lighting adjustment of table saw blade height

From Japan
On 2017-12-20 08:44:19
Although the magnet is small, it is strong and very convenient.
However, as many people wrote, the switch is too small tough ... not to worry about the design, so only knobs on the switch should be bigger.
This review is about item#07063131.
Internal work such as small refrigerator

From Japan
On 2017-08-09 14:52:10
The effectiveness of the magnet is also good, and brightness is enough as it only has to light a point.
Flexi is also satisfying freely.
This review is about item#7063131.
Used when the hand is dark in machine maintenance and product processing

From Japan
On 2017-07-30 00:01:52
It can be used in a narrow and dark place because it is small, and the brightness is just right
This review is about item#7063131.
Purchase expected for hand lighting of lathe · drilling machine · cutting machine

From Japan
On 2017-05-24 15:16:49
Lower light intensity! This is all. It is inconvenient to worry. Batteries are also short. It is necessary improvement. Is it price suitable?
This review is about item#7063131.
Light

From Japan
On 2017-03-24 18:16:55
There is no problem. In addition, I will purchase it if necessary.
This review is about item#7063131.
Shine the tip of the machine's cutlery

From Japan
On 2017-03-07 15:03:16
<Good point> It is cheap. It is light and has adsorptive power, and it is useful for spot lighting of the cutting edge of a machine tool such as a drilling machine, a polishing machine, crossing and the like. It is easy to install and remove, and it can be flexed flexibly so it is easy to get aimed at. <Bad point / Improvement point> Since the switch is small and hard, it is difficult to operate even with bare hands. I want you to be able to operate the switch even with thin skin gloves. Batteries also might be button batteries to lighten the head, but I think that at least AAA can be used.
This review is about item#7063131.
For detailed work

From Japan
On 2017-01-06 08:06:21
It is useful for detailed work. Although the magnet is relatively strong, the switch is somewhat difficult to use.
This review is about item#07063131.
Maintenance check

From Japan
On 2016-10-24 18:18:03
Although the brightness is good, the on / off switch was too fine and it was painful to do.
This review is about item#7063131.
To drilling machine drilling.

From Japan
On 2016-10-12 16:52:01
Magnet is stronger than I thought, even vibration of the drilling machine can not come off. I wanted to focus drill intensively, so this is very good. I will purchase another one for the spot light of the band saw. To put it difficult, it is difficult to switch on!
This review is about item#7063131.
Shine in the box

From Japan
On 2016-10-06 15:42:39
The battery gets split quickly and it gets dark. I wish I could have a few more batteries.
Drill center confirmation

From Japan
On 2016-10-05 22:14:00
It is convenient for brightening the cutting edge of the drill and aligning the center. It is better to be able to install without taking up space
This review is about item#7063131.
Machine maintenance

From Japan
On 2016-09-23 22:46:42
It broke soon. No good. . . . . . . . . . . . . . .
This review is about item#7063131.
Drilling of the drilling board For checking the position of your own work

From Japan
On 2016-05-09 14:49:36
Only points that I want to light up can be confirmed and convenient. However, it is inconvenient because the switch is small. I also want batteries to be AA or enelope-ready.
Checking the size at the time of setting work etc.

From Japan
On 2016-05-03 15:49:15
It is small and does not get in the way I wonder if there is a little more light intensity
This review is about item#07063131.
Confirmation of rust in the tank

From Japan
On 2016-01-13 20:38:04
You may brighter. However, the head is a little big and it is better to be a bit thinner to remove the inside of the tank, but that is a bit expensive.
This review is about item#07063131.
Vehicle maintenance, as a gift for friends

From Japan
On 2015-10-14 16:12:06
I have bought two. One used it immediately for cleaning the engine room at night. It is bright and convenient.
This review is about item#07063131.
Work etc.

From Japan
On 2015-08-22 22:02:17
Because it is flexible with a magnet, the angle is easy to attach, but it was not bright outside and the battery was exhausted. I guess it is useless because it is a button battery.
This review is about item#07063131.