Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hi-La for Steel Pipe Coupling

Hi-La for Steel Pipe Coupling
Sales Price: 16.99 SGD
Review Rating: 4.80
5 Customer Reviews
5 star 4
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
For connection of iron piping
5
From Japan
On 2016-11-14 15:44:14
It gets quite tight. It is good to be able to shorten the time of consolidation work easily
This review is about item#6957632.
Repair connection of piping
5
From Japan
On 2016-03-29 18:21:30
I used it in two places but I was very satisfied.
This review is about item#06957605.
kitchen
5
From Japan
On 2015-12-11 18:04:51
This is convenient, I found this kind of convenient thing in a catalog of monotaro, which I can use for Bowes Kan without having to thread it, I immediately bought it!
This review is about item#06957605.
Piping
5
From Japan
On 2014-12-26 08:54:17
Packing in the inside, ring It can be used without problems. It is useful during piping work. Because the price is also affordable, it is easy to purchase and it is always bought together.
This review is about item#06957587.
In order to attach a valve to existing piping
4
From Japan
On 2014-11-20 14:10:47
I think that it is kind if there is the enclosure of the construction procedure manual, such as the method of driving the lock ring and the installation position of the rubber packing. LA couplings that can be connected without cutting screws also use amateurs in waterworks like me. It does not necessarily confirm the electronic catalog.
This review is about item#06957587.
1
Customer Who Viewed This Item Also Viewed
La Steel Pipe Coupling
LA Coupling HI-LA type
Rubber Packing NBR
Joint Sockets
LA coupling HI-LA type
LA Coupling Adapter
Pipe Connector
Steel Pipe
Inverse seating faucet elbow
La Steel Pipe Coupling
Pipe Coupling