Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of 2 Flute End Mills-Square End With Tialn Coating

2 Flute End Mills-Square End With Tialn Coating
Sales Price: -
Review Rating: 3.47
15 Customer Reviews
5 star 7
4 star 1
3 star 3
2 star 0
1 star 4
The reviews are automatic translation.
Showing 1 - 15 of 15 Reviews
Cutting
3
From Japan
On 2017-03-24 18:16:08
There is no problem. In addition, I will purchase it if necessary.
This review is about item#7226624.
Factory equipment
3
From Japan
On 2015-08-29 11:42:35
Normal upper class. . .
This review is about item#07226667.
On a modeling machine
5
From Japan
On 2015-07-24 23:38:49
I use it in dry because it scrapes wood, but it seems that the cutting edge is torn by the heat so high can not be used, it is very handy.
This review is about item#07226606.
Woodworking work
5
From Japan
On 2015-03-10 07:57:32
I use it with woodworking trimmer. Compared with router bit, finish of plate end face, tenon cut, groove cut and so on, the cut section is sharp and smooth finish can be satisfied. Two blades of long blades and four blades distinguishably from the plate end finish and the deep mortise, the two blades of short blades are distinguished by shallow tenon and groove cutting. I think that it does not change to the finished state with 2 blades, 4 blades.
This review is about item#07226667.
Light metal processing
1
From Japan
On 2014-05-21 14:59:06
No. 2 of the side blade has not escaped, so that chattering occurs on the cutting surface, so it can not be used. Even though I purchased a gash guard type because of similar symptoms before, I mistakenly purchased this time. If you are going to buy gash guard type people can cut it without problems, we recommend that one.
This review is about item#07226667.
Used as mini CNC milling machine cutting tool
4
From Japan
On 2013-03-04 15:50:45
This price is cheap with carbide end mill
This review is about item#07226667.
Grooving into tool steel
1
From Japan
On 2011-11-10 15:38:17
The blade length was 14, but what actually arrived was only about 11 mm. Since it can not be helped it is necessary to polish the blade yourself and make the work in time. I then contacted support and replacement items arrived. But as this was also the same thing, once again telling support, we will now deliver what we have confirmed by measuring from the manufacturer. But this blade length is only about 12 mm. Apparently it seems to be confusing groove length and blade length. Support promised improvement, but until then I think that it is better to purchase with care. (Before that it is going to be out of production · · ·) Also please note that there are strange points in the cutting condition table. Is it that there is a certain risk to cheap ones as well?
This review is about item#07226642.
Mainly cutting of aluminum alloy
1
From Japan
On 2011-09-16 13:22:26
Sharpness of price, sharpness, finish, but there is no particular problem with use. Since the length of the blade length was convenient, it was re-ordered, but the specification changed or the one with the shortest blade reached. In the same way as for replacement, the shorter blade length reached the same way. Looking at other goods, I think that this item will eventually be shifted or integrated to 2TM - 0500 in the discontinued version, but since we are continuously selling, we would like you to confirm and correct the specification etc.
This review is about item#07226651.
Used in cnc milling machine
5
From Japan
On 2011-04-18 22:12:24
It was a cheap and good product.
This review is about item#07226606.
Resin cutting
5
From Japan
On 2011-02-21 10:58:10
Sharpness is bad, there is no sharpness, and burrs remain.
This review is about item#07226676.
Woodworking
5
From Japan
On 2011-02-11 21:11:24
I used it to carve a mortar hole in woodworking, but it was a satisfying feeling of use. As inexpensive, I think I will purchase 2 or 3 pieces as a spare.
This review is about item#07226667.
Resin cutting
1
From Japan
On 2010-06-12 01:31:01
Cutting surface is rough, things that can be cheap, not much.
This review is about item#07226676.
Aluminum milling
5
From Japan
On 2009-01-25 01:11:01
Both durability and sharpness are not enough. It also exhibits considerable sharpness for wood! It is!
This review is about item#07226606.
Milling process
5
From Japan
On 2008-06-21 16:05:45
Damn as much as cheap, dangerous Normal Demo After all the blade holders have only cemented carbide, it was a good product
This review is about item#07226624.
Side processing
3
From Japan
On 2007-11-20 09:37:57
Until now I used the manufacturer's products, but I tried using it. I thought that the work for the price would be enough. Because I am cheap, I would like to purchase again.
This review is about item#07226685.
1