Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Depth gauge

Depth gauge
Sales Price: 46.99 SGD
Review Rating: 4.71
7 Customer Reviews
5 star 6
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
For private, metal processing
5
From Japan
On 2016-08-05 18:37:03
Usability etc. There is no particular dissatisfaction.
This review is about item#07335517.
Dimensioning for changing the brake system
5
From Japan
On 2016-06-13 17:55:13
Taehen can work smoothly
This review is about item#07335501.
Scribe
5
From Japan
On 2016-02-09 15:06:23
good
This review is about item#07335517.
Accuracy check
5
From Japan
On 2013-10-02 17:08:08
It can be used without any problem. I will also purchase it next time.
This review is about item#07335501.
Height measurement
5
From Japan
On 2012-04-11 23:59:38
It is in a wooden case for reasons of low price, and even if it actually looks at the commodity it is comparable to the leading manufacturer. Even if it is used, it is no different from the manufacturer. I think that it is a good product.
This review is about item#07335501.
When scribing the dimensions on the plate material, we use the depth of the gauge as a distance from the board
3
From Japan
On 2012-02-24 00:08:19
In the flat wing which becomes the starting point of the depth, since the central part is about 1 mm down about 10 mm, if the width of the plate is narrow, it will not be used. If you use it as a normal depth gauge, you can not measure the depth if there is not enough surface to be the same. I think that other manufacturers have the same structure. It seems not to be a thing to increase precision or to say that the part has to be lowered by design inevitably, but it is mysterious because it is down as normal.
This review is about item#07335501.
Depth measurement
5
From Japan
On 2011-11-18 13:59:29
It is used for measurement of turning of turning lathes etc. and depth measurement of various things. Until now I measured with the depth of the calipers but since the ground plane is small, the caliper blurred, I could not feel relieved anyhow, but this is still only for exclusive use, the ground plane is stable and accurate measurement can be done I will. It is also a caliper, but the movement of low-priced items is bad is also here. I think that it is a satisfactory commodity from the price if you do not need good things with less frequency of use like a caliper.
This review is about item#07335501.
1
Customer Who Viewed This Item Also Viewed
Digital Depth Gauge
Mini Depth  Gauge
Depth Gauge
Depth Gauge, Straight
Karma Depth Gauge
Karma Depth Gauge
527 series Depth Gauge
0-150mm Depth Gauge
Dial Depth Gauge
Digital Depth Gauge
Carl Mahr type Dial Depth Gauge
Depth gauge regular type
Depth gauge long base
Depth gauge for narrow hole