Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Flattened Can, Double Openings , A Handle, And A Nozzle

Flattened Can, Double Openings , A Handle, And A Nozzle
5 star 4
4 star 4
3 star 2
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Carrying ad bleu
4
From Japan
On 2016-07-20 18:55:53
I am useful because it is the size to enter the tool box. Price is a bit higher than budget
This review is about item#34877832.
For mixing
5
From Japan
On 2016-06-02 20:40:28
Used for mixing gasoline in a mowing machine. There is no problem in particular.
This review is about item#07293885.
For water preservation
4
From Japan
On 2016-04-04 15:35:51
The shape is slim and the space is small, the rotation of the cap is slightly hard, but it may become smooth if you become familiar.
This review is about item#07293885.
I will not buy things from this manufacturer in the future
1
From Japan
On 2014-04-02 19:05:12
It seems that the cap is destroyed on 2nd day of use · bad material is used. Design of the threaded part of the cap is also bad. It's not as complicated as design, but it's not even that simple one.
This review is about item#34877841.
As a detergent container
3
From Japan
On 2014-03-09 16:47:03
Not particularly dissatisfied. Is not the cap durable so much? It seems better not to tighten it tightly
This review is about item#07293885.
Transport of kerosene
4
From Japan
On 2013-11-14 22:16:09
It is used for conveying kerosene for grass burning burner replenishment. A tank of about 5 liters is just right feeling.
This review is about item#07293885.
It is used for supplementing liquid called "Adblue" for reducing NOx contained in truck exhaust gas.
5
From Japan
On 2012-05-30 17:59:54
It is more convenient if there is a cover or cap to avoid contamination of foreign matter such as dust at the tip of the nozzle.
This review is about item#34877832.
In order to carry wash water to places without water supply
3
From Japan
On 2012-03-30 12:52:30
Because the packing is thin and weak, if it is not tightened considerably strongly, water leaks when it falls.
This review is about item#34877832.
Watering the foliage plants.
5
From Japan
On 2012-02-13 13:15:00
Nozzle is a bit hard
This review is about item#34877832.
I use it to put water into the humidifier.
5
From Japan
On 2012-01-27 12:24:30
When wearing an air conditioner in winter, when trying to keep the humidity between 40% and 60%, a considerable number of units are needed, so it is difficult to supply water with kettle or plastic bottles so we introduced this here. When putting in a lot, it seems that water is going to spill while moving from the nozzle side, and there are times when a lot of water suddenly jumps out at the time of water supply, but it is easy to put pouring and put 2L PET bottle to several bottles of water Compared with carrying it is very easy, saving you time and effort is convenient. I think that it was somewhat disappointing that it would be easy to carry size and weight for women as well as for women as well as something about 4 liters, but I was able to save shopping time and labor.
This review is about item#07293885.
I use a liquid detergent in the washing machine as a tank for automatic warming.
4
From Japan
On 2012-01-23 15:28:37
There is not a problem as of now.
This review is about item#34877841.
1
Customer Who Viewed This Item Also Viewed
Plastic Container, with Handle & Small Nozzle
Polyethylene Tank
Polyethylene Tank
Flattened Can, With Single Mouth, Handles And Nozzles
Kerosene Can
Square Cans, Full Open, Handle
Flat Can, with Handle, No Nozzle
Square Cans, Single-Capped, with Handles
For Flat Cans Discharge-Jet Set
Waste Fluid Tank, Nozzle
Universal PE Container
Handy Plastic Tank, Nozzle
PE Water Can
Poritena two mouth
2.0 L poly handy can
Flat Can 20L, Color