Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Lock 22

Lock 22
Sales Price: 28.99 SGD
Review Rating: 4.29
7 Customer Reviews
5 star 2
4 star 5
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
When construction of roof and outer wall
4
From Japan
On 2018-01-24 23:43:05
Because it is not sold to the home center, it was good.
Dimension measurement
4
From Japan
On 2016-02-16 10:39:09
In the past, I ordered with 6 pieces of small boxes (12 pieces), but they were all sent by roses, the packs were dirty, and it seemed like the shipment of the returned goods as it was. Since contents did not have scratches, I used it, but such things lasted about 2 times.
This review is about item#05862141.
Daily work
5
From Japan
On 2015-11-16 08:30:35
I am using it without problems.
This review is about item#05862166.
Black ink
5
From Japan
On 2014-09-12 07:23:03
Easy to use
This review is about item#05246762.
Measurement estimate
4
From Japan
On 2014-08-25 21:41:46
Although I do not use it everyday, I purchase it because I use it occasionally. 25mm is too thick so the size feeling of 22mm is exactly good. It is easy to use with stable quality.
This review is about item#05246762.
Weighing and size confirmation during steel making
4
From Japan
On 2013-04-20 10:20:12
Even if it is extended up to 10 meters upward and surveyed, it does not fold but it is very useful, but after storage at the end of the measurement, it is caught on the scale body etc. at the place of 10 cm, when the used period comes about 1 year or so, It becomes unusable. I hope it will be improved if you see how many such scales are rolling though it can be used for one year.
This review is about item#05246762.
Dimension measurement
4
From Japan
On 2012-10-12 22:51:17
When we measure 8 m and wind it up, I take up the momentum, so it seems to cut off my fingers, so I want the brake function. Because of the width of the tape on the scale, at the time of winding, it was too strong and caught on that side, the tape warped. I want a width of about 19 mm. Although it is natural, it is quite heavy, so it is unsuitable for carrying. I find it useful in long-term measurements at the factory. Because it is Tajima brand, it is safe, but it gets value.
This review is about item#05246762.
1
Customer Who Viewed This Item Also Viewed
Tape measure
G Lock, With A Blister Pack
Tape Measure,
Measure Tape
Measure Tape
Tape Measure
SILVER Measure Tape
Safety Tape Measure
Stainless Lock 22
Measuring Tape
Lock 19, Measuring Tapes
Convex 2 side compact Free 22mm