Customer Reviews of Brazed-Turning Tools
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Lathe processing

From Japan
On 2017-03-24 17:50:23
There is no problem. Also purchase if necessary
This review is about item#7559623.
Cutting processing of resin, general purpose lathe.

From Japan
On 2013-03-03 15:54:12
It is not particularly good nor bad. A little more kind (thanks to resin processing, the chip part is also necessary for high-speed parts) It is appreciated.
This review is about item#07559587.
Used to scrape spot welding electrodes.

From Japan
On 2012-03-02 15:17:40
The angle at which the chip is attached is bad, the second hit, it is impossible to shave. Not available. If you scrape down second, can you use it? .
This review is about item#07559571.
Flat cutting

From Japan
On 2012-02-09 13:30:20
Because the chip is on the table, it has not brazed with a dent. When chatter occurs or the chip becomes smaller and used. . . If continuous cutting is done, heat may accumulate and chips may come off.
This review is about item#07559587.
General lathe machining

From Japan
On 2012-01-24 12:49:38
The angle of the cutting edge was bad (there was no clearance angle in the downward direction on the knife) and it could not cut at all. Do I have to sharpen myself after buying it? I can not do it.
This review is about item#07559596.
Cutting on a lathe

From Japan
On 2011-02-01 19:46:50
The brazed part is dirty, but we purchase it when there is discount. Although it feels like it seems likely to be a little cheaper in appearance. . . There is a time when it is uneasy that the apparent chip can be taken off at the end. Considering the time taken for the first sharpening, there is a sense of merit for the manufacturer's product.
This review is about item#07559571.
Outer diameter cutting with a lathe

From Japan
On 2010-11-23 13:40:33
The tip shape of the shank was distorted and the brazing work was not so good, so the tip was tilted. It was necessary to polish and modify a considerable amount before use. Considering the price difference, might it be better for high cuts? I feel it. I did not have any problem with my left hand purchased together.
This review is about item#07559605.
1