Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Triple Air Coupling

Triple Air Coupling
Sales Price: -
Review Rating: 4.44
9 Customer Reviews
5 star 5
4 star 3
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Distribution of hose
5
From Japan
On 2015-05-31 21:51:53
You may lighten it.
This review is about item#03417154.
For air branching from the compressor
5
From Japan
On 2015-05-03 16:57:39
I can use it without problems. Although it was good with 2 stations, I bought it because it was cheaper for triplets.
This review is about item#03417154.
I thought it was a terminal of air wiring, but it is impossible.
3
From Japan
On 2015-04-19 19:49:00
The plug is squeezed if it does not apply pressure, but when applying pressure, the plug does not insert. I held my head. However, since it became necessary to make three branches in the middle of the wiring, I plan to use it there. I'm glad I did not enter the storehouse.
This review is about item#03417145.
Purchase for branching of air equipment
4
From Japan
On 2015-02-17 22:13:07
Although it is a "triple" air coupling, although three air couplings and photographs can not be seen in the connection angle block, the attachment tap hole of the coupling was opened in the left and right cross section of the square block . So we installed two couplings purchased separately in this tapped hole, resulting in a total of 5 branch couplings. Also, Oscapula was enclosed. Although the blue paint of the corner block was slightly peeled off, it was okay as there was no problem in use.
This review is about item#03417145.
Air duster etc.
5
From Japan
On 2014-10-15 19:52:26
I got lost in the horizontal row type and the circular type, but this time I made it a circular type. It is reasonable that it is compact (and a little cheap) if it is a circular type, because it is easy to insert and remove if it is a horizontal one-row type.
This review is about item#03417154.
Air distribution
5
From Japan
On 2014-05-17 14:21:42
It is cheap and there is no malfunction of the function when using it just because the paint film is thin? I do not know the durability of the coupler, but there is no air leak at the moment
This review is about item#03417154.
Air branch
4
From Japan
On 2013-12-10 17:02:59
It is heavy. There is no problem in use. It is cheap, so what is the durability.
This review is about item#03417145.
I used it in the air piping inside the store.
4
From Japan
On 2013-09-03 20:17:14
It is not bad for the price. so-so. Since it was not bad for taking the first one, we ordered two additional items. I think I will order again if there is opportunity.
This review is about item#03417145.
Working efficiency has improved as multiple air tools can be used without removing the coupler.
5
From Japan
On 2013-07-21 22:24:29
It's good because it does not move easily even if you move the hose because it has moderate weight.
This review is about item#03417145.
1
Customer Who Viewed This Item Also Viewed
Line Coupler 200L
Line Coupler 200 T Model
Line Coupler Rotary Type
Small line coupler
Line coupler type 200S
Universal 3-Branch Coupler
Coupling With Rotary
Branch Coupling, Fixed