Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Glass Funnel

Glass Funnel
Sales Price: -
Review Rating: 3.40
5 Customer Reviews
5 star 2
4 star 0
3 star 1
2 star 2
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
From Japan
On 2016-02-13 07:47:07
I was saved because the small size was hardly sold. Although it was damaged at the arrival, I am satisfied very quickly and carefully corresponding to returned / exchanged.
This review is about item#02913723.
Delicate bottling operation
From Japan
On 2015-07-03 14:46:04
When inserting in a circular mouth container (such as a bottle), if there is something like a groove through which air escapes, it may be poured smoothly. Is it impossible at this price? leg? The part of it may be a little short.
This review is about item#02860672.
Transfer salt to test tube
From Japan
On 2015-03-21 14:31:06
I think that I bought this very well. Easy to use and always clean and secure. I think that the quality was also good
This review is about item#02860645.
Chemistry experiment for college students
From Japan
On 2014-11-28 11:27:25
I bought a funnel with a 45 mm aperture. Although it is very satisfactory in price, I think that it is a problem that the caliber is not the inner diameter but the outer diameter. Glass may be a bit thick, and if circular filter paper of 9 cm is used, it will protrude about 4 mm. Normally, the diameter of the funnel is specified by the inner diameter, so it is natural that if you consider it on the premise that circular filter paper is used (All the things of other traders purchased by us were inner diameter.JIS analysis glass Equipment JIS R3503 is that as well). Packing is polite and conscientious, but with this it will hesitate for future purchases.
This review is about item#02860645.
Preparation of reagents
From Japan
On 2009-10-28 13:38:54
Although it is not a problem that is inevitable in normal use, bubbles and warping are seen in the foot portion, and the cut edge of the foot tip is coarse.
This review is about item#02860663.
Customer Who Viewed This Item Also Viewed
TPX High Speed Funnel
Funnel Base
Micro insert for narrow vials
Powdery Rot
Fine Glass of foot rut
Glass Rot Foot Length Type 60 φ
PP High Speed Funnels
Streak entering funnel
Glass funnel
Glass Funnel