Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pipette Filler, Pie PumpPs

Pipette Filler, Pie PumpPs
Sales Price: 23.99 SGD
Review Rating: 4.00
4 Customer Reviews
5 star 2
4 star 1
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
It is used to dilute the stock solution of the film developing solution.
5
From Japan
On 2018-02-10 18:30:27
It is very pleasant to accurately and easily collect the amount of stock solution, freed from instability of rubber balls
This review is about item#2940262.
Formulation of paint
2
From Japan
On 2016-06-29 18:45:19
I could not read it because the explanation was only in German. I do not know whether it is a problem of making the silicon part of the pipette insertion port, but it hangs up even when I want to suck it up and keep it. For the lever under the wheel, it flows out rather than dropping a minute amount. There was explanation that fine adjustment to the micro range can be done, but it was not true. It was disappointing though it was prepared to some extent because the price was affordable. I hope if you can also write the producer country if possible.
Dispensing operation using a Pasteur pipette with a diameter of about 7 mm
4
From Japan
On 2014-11-02 22:07:52
Like a safety pipettor, it is a tool for safely and conveniently operating a pipette, but it can be operated with one hand, it is a very excellent product in workability because it can perform a sucking / discharging operation like a syringe. Especially useful when dispensing continuously. Somewhat satisfied reason: · Sometimes internal grease up is necessary (not maintenance free) · Spring of the lower part (under the wheel, pushing the lever, opening the valve under atmospheric pressure) is weak or sealing it once it is opened There was a problem that there was a problem that the liquid could not be retained after inhaling (gradually leaking liquid). The latter is not a problem to be troublesome, as we solved the problem by simply extending the spring a little bit and strengthening the force to hold the hemispherical rubber part (sealing the open hole), but if possible improve I would like to ask you.
This review is about item#02940262.
Precision weighing
5
From Japan
On 2014-04-08 01:07:56
good
This review is about item#02940253.
1
Customer Who Viewed This Item Also Viewed
Safety Rubber Pipette
Silicon Safety Pipettor
Micropipette P BOY
Silicon Pipette Filler
Safety Pet
Pipette top
Pipette Aid, Handle Type
PICOLLER Adjustable pipet contoroller
Bioramo short pipette
Macro pipette
NS rubber connection