Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Fine 2-way cock

Fine 2-way cock
Sales Price: 6.99 SGD
Review Rating: 4.27
11 Customer Reviews
5 star 5
4 star 4
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Watering of the plants
5
From Japan
On 2017-08-06 17:40:52
Especially there are no problems, we can achieve our purpose. The packaging was also solid enough to be enough. It was delivered promptly.
This review is about item#2804514.
, During machine maintenance
4
From Japan
On 2017-05-25 20:25:12
The goods arrive quickly from the order and the packing method is also gentle. I will also use it.
This review is about item#2804523.
Stopcap for syringe barrel
4
From Japan
On 2017-03-16 14:57:52
I'd like to use it again because it is reasonable in size and usage, cost performance is also high.
This review is about item#2804514.
Concatenation of hose
5
From Japan
On 2017-02-09 14:40:40
In addition to being firm, it was good, I will also buy
This review is about item#2804532.
Used for supplementing distilled water
5
From Japan
On 2016-08-05 09:26:12
Tigers Polymer Silicone tube 7 mm × 10 mm × 4 m used as a set. It can be used with exactly good size.
This review is about item#02804523.
Stop valve for outside air release for piping filter part
3
From Japan
On 2016-04-15 18:02:35
Plastic valves are good because they are somewhat corrosive liquids
This review is about item#02804523.
Equipment for hydroponic cultivation
5
From Japan
On 2016-04-04 18:33:04
It was used as a cock of a liquid fertilizer mixing apparatus of tomato's hydroponic culture, but it is inexpensive and very appreciated.
This review is about item#02804514.
Making teaching materials
3
From Japan
On 2015-06-05 21:18:27
I purchased it for trial at Dame Moto trying to use it for a valve at a place slightly higher than the atmospheric pressure, but when the cock was operated the air leaked out. Because it is not a substitute for stopcock, those who are being examined are cautious.
This review is about item#02804523.
Used between hoses
4
From Japan
On 2015-01-20 14:24:05
It can be used normally. It's better if the total length is shorter
This review is about item#02804532.
For adjusting flow rate from drip container
4
From Japan
On 2014-08-05 14:29:36
I purchased it because it is less expensive than metal. I see how it can be used for a long time.
This review is about item#02804523.
Currently, I am using it for old because I am using it.
5
From Japan
On 2014-06-10 13:42:17
I can save it if I can clean the middle.
This review is about item#02804523.
1
Customer Who Viewed This Item Also Viewed
Luer Stopcock
Roller Clamp
LAB Cock Hose x Hose
Tube Clamp
Three Way Stop Cock PE
Fine Irrigator Pe
Two way stopcock (PE)
Two way stopcock (PP)
Hose Coupling Set
Mini Coupling
Two way stopcock
Mini Coupling
Fluororesin two way cock
Stopcock (PP)
Minibarubu
Cock Steel