Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Spoon - Stainless Steel

Spoon - Stainless Steel
Sales Price: 1.99 SGD
Review Rating: 4.22
9 Customer Reviews
5 star 6
4 star 1
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
When painting work
3
From Japan
On 2017-10-19 16:46:39
I think that it is good for your valuable and good. . . . . . . . .
This review is about item#02910896.
For sampling powder products
4
From Japan
On 2017-06-11 11:50:33
As described elsewhere, I care about the edge of the handle part. It is easier to use a more rounded one.
This review is about item#2910844.
Take out the paintings of Japanese paintings from the bottle
5
From Japan
On 2017-01-13 19:02:15
This medicine spoon is the easiest to use when taking out rock paint and water paint from a paint bottle of Japanese painting. It is recommended for those who draw Japanese paintings.
This review is about item#2910792.
Kitchen, kitchen work
5
From Japan
On 2016-10-27 08:54:00
Here, something useful, I use various sizes in the kitchen. There are fewer recesses than ordinary spoons, which is useful to scoop paste-like objects.
This review is about item#02910896.
Mix salt る
1
From Japan
On 2016-03-14 16:50:27
Because I do not round the corners of the handle, my fingers hurt so hard to use. The company's spoon made of 240 mm bought at the same time rounds the corner of the handle. 360 mm keeps high as much as 5 times as high as that, yet it is omni-directional. Also, since the angle of the scooping part is small, it is difficult to scoop (this point is the same for 240 mm). I would like to feel obliged to throw a circle without direct instructions on subcontracting.
This review is about item#02910853.
Actually it is being used for ordinary edible
5
From Japan
On 2016-01-16 15:58:23
Unlike the existing spoon, the width is thin so it is very useful for taking out bottles of food. Especially jam is the best. When scooping a jam and putting it on bread, it is very easy to paint because the bulge of the spoon itself is modest. Also recommended for powder juice (originally easy to scoop for chemicals) even better is the length. It is easier to use because it is longer than a normal spoon. I think that there is resistance before using it because it is a drug spoon, but it is pretty good to use.
This review is about item#02910896.
coffee
5
From Japan
On 2015-09-21 21:43:27
I am in an instant coffee bottle. 150 mm is the easiest to use.
This review is about item#02910896.
cooking
5
From Japan
On 2015-07-12 21:56:19
I purchased several pieces to cook condiments and taste during cooking. It also leaves something after scooping the hardness like jam, it is easy to wash. I am more user friendly than teaspoon and I liked it very much as I had it.
This review is about item#02910792.
Make cosmetics
5
From Japan
On 2015-05-28 18:32:15
It was good as I was thinking.
This review is about item#02910817.
1
Customer Who Viewed This Item Also Viewed
Spatula Spoon
Spoon
Laboratory Spoon, Spoon
Lab Spoon
Long muddler spoon
spoon
Straight muddler
Scoopula (stainless steel)
spoon
Spoon
  • Spoon
  • Tokyo Glass Kikai (TGK)
  • 1.99 SGD
  • 5.000000(1)
Spoon small ST