Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Skill touch - offset type - stone material - for glass

Skill touch - offset type - stone material - for glass
Sales Price: 3.99 SGD
Review Rating: 3.83
6 Customer Reviews
5 star 3
4 star 1
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Tile joint
3
From Japan
On 2016-04-14 20:09:21
I think that it is used for finish cutting of tile joints, but it is still unused. I do not get a feeling.
This review is about item#05587592.
Repair of side mirror of motorcycle
5
From Japan
On 2014-11-04 21:40:35
I used to cut out the convex mirror to just the right size. It was difficult because glass was put on it unless it was scraped carefully, but it worked well. The price is also cheap and it seems to last a long time as much as cutting thin glass. I bought rough things of the same number at the same time but it was not suitable for sharpening thin glass.
This review is about item#05587583.
I am using it to make the quartz shape.
5
From Japan
On 2014-05-12 18:59:07
It is useful for determining the shape.
This review is about item#05587583.
Finish the pottery
5
From Japan
On 2013-12-23 17:42:35
I made pottery but used to scrape off the soil and to fix the glaze dripping. It reduces crack cracking time and does not feel stress.
This review is about item#05587583.
Polishing of ceramics etc
4
From Japan
On 2010-07-01 22:22:41
Is good
This review is about item#05587601.
Glass cutting
1
From Japan
On 2010-01-20 18:36:34
I purchased a transparent glass plate (t3) to shave it about 1 mm. (Shaved length is about 80 mm) (It is difficult to cut 1 mm with a glass cutter.) Although there was no major collapse, it could not be cleaned beautifully. It seems that the side part is wavy, the cutting trace is biased to a part, probably because of that. If you want to cut the glass cleanly, it seems that a grinding wheel dedicated to glass is good.
This review is about item#05587583.
1
Customer Who Viewed This Item Also Viewed
Techno disk C
High Wrap Offsett Whetstone
Pad for Grinding Wheel
Techno disk LL-C
Cut Off Wheel
Skill Touch R-2 CC16 125
Cutting Wheel
Ceramic Grinding Wheel
Offset Grinding Wheel
Insulating coating with crimping terminal closed end connector