Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Small Pressure Gauge

Small Pressure Gauge
Sales Price: 19.22 SGD
Review Rating: 3.89
9 Customer Reviews
5 star 6
4 star 0
3 star 1
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Small compressor pressure gauge
5
From Japan
On 2017-02-06 16:27:40
Satisfied, purchased as an exchange for damaging the same thing.
This review is about item#2001115.
Machine pressure display
1
From Japan
On 2016-08-29 22:28:16
There is an outer diameter of 40 mm, but even the smallest part you received reached 42 mm strong, the maximum part is 44 mm or more. Please display accurate dimensions.
This review is about item#2001115.
Fuel tank pressure
3
From Japan
On 2016-08-14 11:28:25
It works without reality Problem It is good if there is a difference in position of the mounting part
This review is about item#2001133.
Product installation for pneumatic pressure measurement
1
From Japan
On 2016-08-13 11:32:38
Although there was no problem in function, the glass surface of the pressure gauge was full of scratches. I did not think that it was packing very precisely with just packing it put in three pieces randomly into a plastic bag. It is almost like handling of screws and nuts.
This review is about item#2001142.
The pressure gauge which was an accessory at the time of repairing the equipment was bad and needed to be exchanged
5
From Japan
On 2016-07-25 16:57:33
Even compared with old products, there was no big difference, there was no discomfort.
This review is about item#60854437.
For tire pressure gauges for off road bikes
5
From Japan
On 2016-06-14 20:44:52
The tire air gauge ready-made goods corresponding to this pressure range (0 ~ 0.1 MPa) is less cheap than it is, so I bought it for my own work purpose. For industrial use, measurement accuracy is very good. When you want to adjust the needle by proofreading etc., it may not be easy to detach it because the lid is not screw fixing.
This review is about item#02001115.
Gauge of tennis ball pressure case
5
From Japan
On 2016-03-05 17:54:53
Detailed pressure is displayed and it is very convenient. Even if we receive a little external force, it is solid and it can be used with confidence.
This review is about item#02001124.
Painting work
5
From Japan
On 2015-11-02 21:10:20
Replace with a pressure gauge of a monotary regulator. I wanted to use it at low pressure, so this is convenient. The pressure gauge attached to the regulator of the monotary is slightly blurred, but this is stable steadily.
This review is about item#02001133.
I used it for boost pressure test
5
From Japan
On 2015-10-26 18:39:17
Although it was good to attach it to the testing machine used for the pressure test inside the suction pipe of the turbo car, it is fixed directly to the suction pipe because it likes instruments The test is completed without delay, of course the measured value is also electronically boosted It is equivalent to the meter It is convenient now that the pressure inside the piping can be understood without having to go back and forth between the inside of the car and the engine room Is the problem moving properly the next time it is used Since the installation place is in front of the turbine Although the temperature of the gas entering inside the pressure gauge will not be a big deal, it should be an environment of 60 degrees or more, so it is only worrisome there if there is clear it If you can clear it please purchase another one and this time to the surge tank I intend to attach
This review is about item#02001124.
1
Customer Who Viewed This Item Also Viewed
Pressure Gauge
Small Pressure Gauge
Pressure Guage
Small Pressure Gauge A form Vertical phi40
Pressure Guage
Small Pressure Gauge
Small Pressure Gauge
Small Pressure Gauge
Small Pressure Gauge (Vertical-collarless)
Compact Pressure Gauge
Compact Pressure Gauge
Compact Pressure Gauge
Embedding Type Pressure Gauge A Class phi50