Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Fixed Grip

Fixed Grip
Sales Price: 4.99 SGD
Review Rating: 4.40
5 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
As a machine tool custom
From Japan
On 2017-10-05 23:10:03
The real thing was sharp and good thing from this product picture Unfortunately it was disappointing that there were 2 mm scratches that stand out.
This review is about item#7005512.
Used for adjustment handles of old machine tools
From Japan
On 2017-08-08 10:24:48
I think that making is solid, I do not have Bali. The installation handle is below, I bought it with a monotaro. V100 - H14 morning glory handle car (with shaft hole processing) with female thread for gripping Imao Corporation 21585314
This review is about item#7005476.
Attach to Hitachi stirrer
From Japan
On 2017-07-21 09:06:09
Attach to Hitachi stirrer I used it to mix mortar and concrete with stirrer Since it seems that installation availability will be divided by manufacturer How about being ordered by looking at the screw diameter? I bought a used stirrer There was no grip I thought that I could use it as it is I will take each body as plainly as I can There was a lot of burden on wrists, arms and waist Judge the grip as unreasonable as not expected So this is a cool grip Very hard, healthy, cheap The burden on the body is ultimately relieved than anything else The grip seems to be used longer than the life of the agitator liked it Person who got damaged, who lost It is a recommended item
This review is about item#7005512.
Milling machine
From Japan
On 2016-03-14 18:29:56
It is used for dialing of milling machine. It began to adjust to precision. It is also planned to be used for small lathe dial.
This review is about item#07005476.
Electric grinder handle
From Japan
On 2014-03-19 18:35:02
The length is also appropriate and satisfactory.
This review is about item#07005327.
Customer Who Viewed This Item Also Viewed
Steel Grip
Stainless Steel Fixed Grip
Bar Grip
Rotating Grip
LDMS clamping lever (male thread)
Plastic Fixed Grip
Plastic Pillar Grip
Stainless Steel Rotation Grip
Rotating Grip PP
Rotating Grip
Fixed Grip, Female Screw
UAF aluminum handle
Rotating Grip