Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Wide Screw Shackle

Wide Screw Shackle
Sales Price: 8.99 SGD
Review Rating: 4.80
5 Customer Reviews
5 star 4
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Lifting operation
4
From Japan
On 2017-10-13 17:28:47
It is going to be used when lever block is used. I did not have to be stainless steel. I wanted galvanized galvanizate if possible.
This review is about item#6913532.
Crane work
5
From Japan
On 2017-07-06 16:26:54
It is used for crane work using nylon sling. It is just snug because the width of the nylon sling is 25 mm. There was no stock in the nearest mass merchandising store, and it was saved because I was able to order from mail order.
This review is about item#6913523.
Redundant repair
5
From Japan
On 2016-08-14 17:46:26
It was convenient to use for repairing hanging metal fittings of a large-sized blind
This review is about item#6913523.
For mooring a boat
5
From Japan
On 2016-07-26 16:13:25
Wide - type shackles are not sold inside, and even if they are sold, they are expensive, but they are cheap and saved.
This review is about item#06913541.
Lifting up objects of about 300 kilograms (combined with chain block)
5
From Japan
On 2015-02-20 13:18:35
There is no particular problem in use feeling. Size etc It was stated properly so we were able to purchase with confidence.
This review is about item#06913541.
1
Customer Who Viewed This Item Also Viewed
Stainless Steel Screw Pin Anchor Shackle
Long and Wide Screw Pin D-Shackle
Screw Shackle
Flat Shackles
Stainless SLU shackle
Stainless Steel Shackle
Stainless Aiborutobuneji
Wide Screw Shackle