Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Liquid Level Relays Standard Set

Liquid Level Relays Standard Set
Sales Price: 129.99 SGD
Review Rating: 4.50
2 Customer Reviews
5 star 1
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
Used to stop the pump automatically when irrigating crops from aquarium with a motor pump
From Japan
On 2016-07-27 07:17:15
It was very easy to use with the same product as the product I used before. It was saved by having the same product as a monotaro.
This review is about item#06945416.
Water tank control
From Japan
On 2016-05-20 16:10:23
It was adopted for pump ON and OFF at draining. The relay is a simple structure for turning on and off the microswitch by buoyancy, and if it is less than the allowable current value of the microswitch, load control can be done directly with this relay so it is simple. The weight that utilizes buoyancy can be arbitrarily adjusted with strings on the lower side and the upper side, so it only determines the position according to the depth of the tank. As for the improvement plan, it is easier to make the adjustment by making a hole through the center of the weight attached to the upper surface of the two weights so that the weight can be fixed to an arbitrary position. This time the string was positioned outside the weight and positioned, so the string is not connected individually as shown in the illustration of the manual. If you have such a simple structure I think that you can lower the price a little more.
This review is about item#06945416.
Customer Who Viewed This Item Also Viewed
Float Switch
Float Level Switch
Quick Float
Quick Float
Relay Adapter
TBL1 series
Nissui liquid level relay body
Water level sensor kit
Float Switch, Level Control