Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hybrid Screwdriver No.5300

Hybrid Screwdriver No.5300
Sales Price: 21.99 SGD
Review Rating: 5.00
1 Customer Reviews
5 star 1
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 1 of 1 Reviews
Removing the screw secured to the aluminum frame and securing the screw
5
From Japan
On 2013-10-18 08:40:27
Up to now I have bought a penetrating driver for about 5 years, but this is done with only one budget It is satisfactory even with the bit attached to the standard but the bit is using Bessel This is the strongest combination This is the strongest combination of vessel High precision bit and this sun flag 5300 You can definitely get the screw even if you do not use impact Impact Somewhat satisfied with 10% off in monotail but it was the same as price at home center I am satisfied with the amount only by the point
This review is about item#05848735.
1
Customer Who Viewed This Item Also Viewed
Hybrid Grip Driver No.5700
Hybrid Grip Driver Replacement Bit
Telescopic Driver, SUNFLAG
2WAY Screwdriver
SF # replacement for the 5800 bit
Bolster Screwdriver
Magnet ratchet driver
8way Universal Driver
Interchangeable Screwdriver Set
Replacement cushion driver
Commercial Grip Screwdriver
Perfect Cushion Grip 2WAY Driver