Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Angle Shank Type Chamfering Cutter

Angle Shank Type Chamfering Cutter
Sales Price: 68.99 SGD
Review Rating: 4.60
5 Customer Reviews
5 star 4
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Ali processing
3
From Japan
On 2017-08-01 15:01:35
Because there are many blades, I thought it would be beautifully finished and purchased. A cemented carbide blade might have been better.
This review is about item#7692343.
Slitting at 45 degrees
5
From Japan
On 2017-04-09 21:30:47
There are many teeth of 45 degrees, so we were able to clean up beautifully.
This review is about item#7692036.
Ali groove processing and surface cutting
5
From Japan
On 2010-01-25 00:13:40
Originally I bought it for use only for dovetail groove machining, but I also use it for surface machining by milling as it has a sharpness. Surprisingly convenient for surface processing.
This review is about item#07692316.
Production of precision parts for sports using aluminum material
5
From Japan
On 2009-06-16 20:05:49
I also like it in terms of size, is the machining more stable as the spindle is slightly thicker (12 Φ)?
This review is about item#07692316.
It is used for cutting hard aluminum (T-6). ⇒ Making parts for precision machinery.
5
From Japan
On 2009-06-01 17:03:50
If you frequently remove the facet, the degree of scraping is satisfactory. As an improvement request, ① Lengthen the length of the handle by 10 mm ② I want the case to be a little bigger.
This review is about item#07692316.
1
Customer Who Viewed This Item Also Viewed
T-Slot Cutter
Double Angle Shank Type Cutter
Carbide Arigiri
Single angle cutter
T Slot Cutter
W With Angle Cutter with Pattern
Umbrella cutter with handle
Key sheet cutter