Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Tie Mount

Tie Mount
Sales Price: 15.99 SGD
Review Rating: 4.43
7 Customer Reviews
5 star 4
4 star 2
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Bondage of coaxial cable and VA cable in board
5
From Japan
On 2014-12-21 14:36:24
Very good. Even if the tightening direction goes up and down, you can change it even if you are left and right. Can be fixed with a single 3.5 mm countersunk screw, economical.
This review is about item#08038152.
Air conditioner
3
From Japan
On 2014-05-09 14:02:58
There was nothing wrong.
This review is about item#08038161.
Mechatronics
5
From Japan
On 2014-02-10 16:32:49
It is useful because you can secure the wire securely with screw fastening.
This review is about item#08038152.
Wiring work
5
From Japan
On 2013-05-24 08:34:48
good
This review is about item#08038195.
Wiring around the PC
5
From Japan
On 2013-01-09 10:56:50
I screw it to the back board of a wooden computer desk and bundle the lines and use it for arrangement. It was surprising that the lines of two desktop PCs and three monitors were organized cleanly. It is convenient because you can change the length of the band according to the amount of the wire while keeping the mount. In addition to the PC desk, the wiring of the television board in the house was cleaned up neatly. I am satisfied that the appearance is good. I think that it should be 50 pieces as it is used in hobby.
This review is about item#08038222.
Fastening of the electric wire in the electric board
4
From Japan
On 2012-10-16 17:35:04
The double-sided tape method which I used until now may be removed soon so I tried it. It takes a while to install, but a sense of security that does not come off is very good.
This review is about item#08038204.
I use it to fix electric wire and piping.
4
From Japan
On 2010-03-19 09:23:12
Unlike the sticky mounting base, it fixes with screws, so I think that it has a fixed strength. I thought that it would be good if there were duplicate items.
This review is about item#08038152.
1
Customer Who Viewed This Item Also Viewed
Black Cable Tie
Super-grip cable tie mounts
Self Adhesive Tie Mount
Tie Mounts, Self-Adhesive
Mount Base
Cable Tie Mount
Cable Tie Mount
Mount base (screwed type)
Tie Mount
Thailand mount (KR)
Anchor Mount
Tie Mount Holder
Cradle
  • Cradle
  • HellermannTyton (former Tyton)
  • 21.99 SGD