Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Single Point Diamond Dressers

Single Point Diamond Dressers
Sales Price: -
Review Rating: 3.20
5 Customer Reviews
5 star 1
4 star 0
3 star 3
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
As a dresser
3
From Japan
On 2017-03-24 17:34:03
I am using, but there is no problem. We will also purchase
This review is about item#8239506.
Formation of whetstone
3
From Japan
On 2013-06-03 16:31:29
It is saved when 8 mm - 100 is available.
This review is about item#08239481.
Polishing and scribing
2
From Japan
On 2012-12-13 14:17:39
I used it attached to the milling cutter, but it was not so because core did not come out. Also, it is easy to match the application as it is displayed in the instructions as if it were raw stone, or the shape of the scoop or conical scoop.
This review is about item#08239481.
Surface conditioning of centerless polishing whetstone
3
From Japan
On 2012-06-27 16:59:05
I searched that it would not handle it, there was. It is a monotary stone. I was able to successfully face it without problems. Compared to what I used to use, the diamond is about half as small as I was concerned. I used it after cutting the shaft because the shaft is long.
This review is about item#08239497.
Grinder dressing
5
From Japan
On 2011-03-01 09:27:34
Satisfied because it can be used normally
This review is about item#08239497.
1
Customer Who Viewed This Item Also Viewed
Diamond Dresser
Diamond dresser
Diamond single stone dresser
Diamond single stone dresser
Donut dresser (for replacement)
Donut dresser (for surface grinder)
NEW LL single stone dresser
Diamond single-stone dresser