Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Interchangeable Stamping Set

Interchangeable Stamping Set
Sales Price: -
Review Rating: 4.33
3 Customer Reviews
5 star 1
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Engraving on leather and metal
From Japan
On 2012-11-02 17:06:37
Plastic positioning frame, very convenient.
This review is about item#08252711.
Marking on metal products Attached to a self-made jig and stamped with a press machine
From Japan
On 2011-11-10 00:24:03
Distribution of numbers, letters, etc was the best. If ordinary 2 sets necessary place I was worried about the variation in width and height because it was made in Taiwan made in this set, but it was uniform uniformly. It is regrettable that there is only a character height of 5 mm. Please release 3 mm version by all means. Since it is also expensive, please consider rose selling as well. I think that it is convenient to put out the things necessary for engraving if you make it a double bottom so that the sponge part which will be engraved at the end is made
This review is about item#08252711.
For sorting processed goods
From Japan
On 2007-12-11 13:59:02
It is convenient to strike cleanly with a holder. Because there are multiple each, mostly it is in time.