Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Drill case

Drill case
Sales Price: 13.99 SGD
Review Rating: 4.30
10 Customer Reviews
5 star 6
4 star 2
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Woodworking · Iron Works
4
From Japan
On 2017-10-22 18:58:33
Fujikoshi and Mitsubishi Materials are used for general iron drills, The length is perfect and it is very easy to use. The 25 bottles I bought are made up of 3 rows, Bits in the same column are designed to be aligned at the same height and are easy to retrieve. Although it is good to raise a bit with opening and closing operation, but a bit of movement is awkward, Until you get familiar, it seems that you have to hold the case firmly and open and close it.
This review is about item#8279092.
At processing on site
3
From Japan
On 2017-05-23 20:52:59
Although I was using the same thing before, it is easy to break the instructed point of the case to insert the dust
This review is about item#8279092.
Organizing taps and drills
5
From Japan
On 2017-05-10 18:07:20
You can organize taps and drills of typical sizes and use them conveniently. If possible, you can put more than one handles if you can make the space for tapping the handle a little bigger, I think that it is convenient because you can transport the tool only in this case.
This review is about item#8279126.
Organizing drills
5
From Japan
On 2017-05-10 18:02:47
I can organize drills of a typical size and use it conveniently.
This review is about item#8279092.
Used to organize taps
4
From Japan
On 2017-01-28 21:44:55
I was saved because the tap size was sorted out apart. Since the ratchet wrench does not enter the handle storage, I want it to be a little wider. As for tap storage, I do not want tap for impact driver and I want you to change it.
This review is about item#8279126.
Organizing drill blades
5
From Japan
On 2016-08-21 21:30:48
Although I searched in the home center, I was suffering without cheep things, but I found out what I wanted and I am satisfied.
This review is about item#8279092.
Used for storing small diameter drill and milling end mill
5
From Japan
On 2015-11-17 18:43:07
Price is reasonable, quality is good. The outside is a solid metal case, the drill storage block is a smooth, foldable resin structure of movement, reasonable construction. It is easy to check and remove the dimensions of the drill when opening the case.
This review is about item#08279117.
To organize the drill's blades.
5
From Japan
On 2014-05-06 20:21:04
I am satisfied that the construction of the case is firmer than I thought.
This review is about item#08279117.
Drilling and tapping work
2
From Japan
On 2013-07-24 19:38:50
The hole for tapping is small, and if it is not enlarged, the tap does not enter.
This review is about item#08279126.
Organize
5
From Japan
On 2011-04-25 13:30:06
It is convenient to find tenderly It is a square shape with a wasteful design so it is convenient to close in the tool box and it is very handy.
This review is about item#08279117.
1
Customer Who Viewed This Item Also Viewed
Drill Stand
Rotation drill stand
Ironwork drill set
Drill case
BSK End Mill Drill Case
MRV Long pack case
TPK Tap Case