Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Cushion 4 way stub driver

Cushion 4 way stub driver
Sales Price: 9.37 SGD
Review Rating: 4.40
5 Customer Reviews
5 star 3
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Motorcycle maintenance
5
From Japan
On 2017-10-13 14:45:38
Actually this is the 2nd generation, the former was broken. It is easy to grasp, it is easy to apply force. Since it is troublesome to exchange bits, I have two plus and two minus (lol)
This review is about item#8433363.
household use
4
From Japan
On 2016-04-20 22:26:57
It is very nice to be able to use four kinds of + - drivers with that small size. As a part I would like to improve by only one point, since there are few places to grasp when changing from a small size to a big size, I think that there is some countermeasure if the finger hurts.
This review is about item#08433363.
Maintenance of car parts
5
From Japan
On 2015-11-13 12:50:07
Even if it is a narrow place, if it has one, it all covers. Bonus small because it is a tool box, it is recommended item No. 1 to use.
This review is about item#08433363.
Building maintenance
3
From Japan
On 2015-10-30 11:49:10
It is convenient for carrying.
This review is about item#08433363.
It is convenient when opening the control panel.
5
From Japan
On 2015-01-26 22:22:23
As I usually opened the control panel and connected the computer etc., I put ordinary drivers in pants pants, so holes were coming and I was getting angry at home. I wish I had bought it before this if it was so convenient. I think the purchase price is also very good.
1