Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Mold Knob

Mold Knob
Sales Price: 2.99 SGD
Review Rating: 4.60
5 Customer Reviews
5 star 4
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
VTR for Panasonic HD studio Voice input dial of model number AJ - HD 1600 was missing and it was used for repair.
From Japan
On 2017-04-06 19:04:44
This time, we are using it, because the volume input dial of the HD VTR for Panasonic studio was missing, I searched for something similar in size and shape, so I found exactly the right thing so here I installed it carefully. A little, because the shaft on the VTR side is thick, it was remodeled.
This review is about item#8626274.
For inverter speed change
From Japan
On 2015-11-30 22:10:42
It was small and good as far as the outside of the control panel
This review is about item#08626274.
Inverter speed switching
From Japan
On 2015-03-11 07:58:17
It is inexpensive and easy to use.
This review is about item#08626274.
Headset for bike radio
From Japan
On 2014-10-24 15:06:33
Shipping was also saved soon. I want to use it again.
This review is about item#08626265.
Arm light switch knob cover
From Japan
On 2013-02-08 10:03:37
At the hospital, I purchased it as a substitute for the knob (cover) attached to the switch part of the arm light in the hospital room. However, the shape of the switch part differs depending on the manufacturer, it was unusable. One is a mountain type, the tip is 6.1 mm, but the former is 6.3 mm and only the tip is entered and the second is the same diameter (6 mm) but there is a part flat part but not spun state was. Previously I asked the manufacturer of the arm light to sell the parts, but as I was easily refused, I was looking for an alternative item.
This review is about item#08626274.
Customer Who Viewed This Item Also Viewed
Mold Knob
Mold Knob Cap
Metal Knob K-5475
Mold Knob K-1
Mold Knob K-3
Metal Knob K-29
Knob (for ultra-compact rotary)
Mold knob K-75
Mold Knob K-2605
Mold Knob K-2901
Mold Knob K-4071
Mold Knob K-5380-A
Mold Knob K-6
Metal knob K-50
Metal Knob K-5424
Metal Knob K-5432
Mold Knob Disk K-100
Mold Knob K-2670