Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Safety Semi Stainless Steel FS Type

Safety Semi Stainless Steel FS Type
Sales Price: 1.99 SGD
Review Rating: 4.90
10 Customer Reviews
5 star 9
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Fastening of hose
5
From Japan
On 2017-05-06 14:41:21
You can work with confidence because the cover is attached. Tightening is no problem.
This review is about item#8676884.
It was just right length and width.
5
From Japan
On 2016-10-27 13:55:07
Although it was a secured band of the radiator hose used before a long time, it was a type that bent a narrow steel tubular object and closed with leaving two thin securing marks on the radiator hose but it passed the year And the cooling water leaked delicately from the part of the secured bond and it became a state not interesting as a maintenance side. In order to solve it, as much as possible on the occasion of radiator hose as a new item, I had to exchange for this hand and waited for a wait. Although there are things that have passed for several years, there is no big trouble and leakage does not occur and I am following very good progress. To be honest, as for the over-tightening, there is worry that it will split if the radiator side is Plus Tech, but if you stop at a place that stops with a short ratchet wrench, I think that the problem will not occur.
This review is about item#8676884.
Fixing of rubber hose of air piping etc.
5
From Japan
On 2016-10-21 14:30:35
The processing of the end face of stainless steel is good, it can be tightened strongly, the performance is sufficient, since the hole to be tightened is not opened by the press, the rubber does not bite into the hole of the screw when tightened so that the surplus metal part Since the cover is attached to the end face, I think that it is a good product even in safety, that it is no longer injured.
This review is about item#8676893.
Air hose stop
5
From Japan
On 2015-08-27 14:51:02
Even if you tighten it until it is convincing, the band will not break. Burr treatment of the band is also nice for the hose.
This review is about item#08676866.
Used for cooling water hose band of car
5
From Japan
On 2015-08-26 07:46:38
It is perfect fit and easy to use, the fastening part is + and usability best.
This review is about item#08676893.
Mounting hose
5
From Japan
On 2015-05-12 14:43:04
Be firm
This review is about item#08676893.
Connection of sea water cage hose circuit hose
5
From Japan
On 2014-11-19 21:21:42
I was able to install with confidence with a firm thing.
This review is about item#08676893.
Lotus conservation work
5
From Japan
On 2014-09-27 06:35:32
It's very nice.
This review is about item#08676893.
To the connection
4
From Japan
On 2011-04-28 22:46:48
Especially no problem
This review is about item#08676927.
Hose for liquid pumping pump
5
From Japan
On 2008-08-23 17:05:17
Durable and tightened many times, it is very satisfactory because it is hard to break even when repeating loosening.
This review is about item#08676884.
1
Customer Who Viewed This Item Also Viewed
Hose Clip SS
Normal Hose Grip
Mini Clamp,SUS301
Hose Clips SUS
Steel Hose Clamp
Safety Hose Clamp