Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of HIGH PITCH PAPER HN TYPE

HIGH PITCH PAPER HN TYPE
Sales Price: 47.99 SGD
Review Rating: 4.00
7 Customer Reviews
5 star 4
4 star 1
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Automotive painting
3
From Japan
On 2017-11-17 22:21:22
I think that it is better to have compared with other manufacturers, so I will purchase again.
This review is about item#8726365.
Iron polishing
5
From Japan
On 2016-03-17 15:09:08
Easy to use and easy to use
This review is about item#08726313.
To automobile sheet metal
4
From Japan
On 2015-10-12 21:05:11
I do not think so specially.
This review is about item#08726331.
Peeling of coating film
5
From Japan
On 2015-04-07 09:18:35
I am very satisfied. I am planning to make a continuous purchase.
This review is about item#08726313.
Car sheet metal
5
From Japan
On 2014-03-07 11:49:38
no problem. I bought it at a paint shop but it was cheap so buy it here.
This review is about item#08726331.
Finish the weld beat with Thunder, and finish the final at No. 120
5
From Japan
On 2013-11-28 13:14:29
I am very satisfied when using it
This review is about item#08726331.
FRP bottom painted undercoating
1
From Japan
On 2011-06-10 13:29:02
Although there is no problem for usual use on the side of the abrasive material, adhesion strength on the magic side is not good. I installed it with three models, but none of the magic side's attachment power has gone before the paper's lifetime. Please increase the thickness a little more or consider the material. It seems that the durability of the abrasive is so abundant that I think that this is a little wasteful.
This review is about item#08726295.
1
Customer Who Viewed This Item Also Viewed
Sanding Paper,
Magic Disc, Perforated
HIGH PITCH PAPER HN TYPE
Rapid pace paper HR type
Sanding Paper,
P pot 3 L set
Air Sander Paper
Disc Grinder
PS paper PN type
Abrasive Paper
High Pitch Green
Sanding Paper,
High Pitch Green
Hi-Pitch Paper, J5 For Air Use, Sold Separately
High Pitch Green
PS paper PR type
High Pitch Paper Hnas
Disc Grinder