Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Drill Bit Sharpener

Drill Bit Sharpener
Sales Price: 51.99 SGD
Review Rating: 2.33
9 Customer Reviews
5 star 1
4 star 2
3 star 1
2 star 0
1 star 5
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Drill polishing
3
From Japan
On 2015-10-06 10:24:07
I can use it for the price.
This review is about item#08756167.
Drill regrinding
1
From Japan
On 2015-01-15 13:52:27
Put the tip of the drill in the hole of the guide and polish it 180 degrees on each side, but no drill center at all. It can not be polished equally on both sides. Holes can not be drilled in the drill polished state as it is. Since the window is open so that it can be polished at the outer periphery of the grinding stone on the side, it is useless unless you polish it again by hand. I could have just bought a grindstone to do this.
This review is about item#08756167.
Regeneration of drilled bit of cutting edge
5
From Japan
On 2014-02-07 18:53:28
Lightweight and compact usability is also satisfactory for now. What will happen if the whetstone wears, the future is a game.
This review is about item#08756167.
Correction of drill bit from tree to stainless steel
4
From Japan
On 2014-01-08 17:46:08
I also want Hokkaido to match from the beginning. But whatever the drill bit it opens up to what hole. The meaning changes. It is an opponent. With or without drill paste. Although it was better to have it. For example, if you turn the blade red, it will be finished in one shot. rear. There is a sharpening fee, it is inside! It is not to see a dream. It only needs to improve the sharpness. It depends on how far you work. It is not a tool that a poor person can use, and it is useless.
Drill's teeth regeneration
4
From Japan
On 2013-03-12 09:33:02
I want you to improve like a keyless chuck
This review is about item#08756167.
Cutting operation
1
From Japan
On 2012-10-17 16:42:15
It is completely useless at all. I do not understand how to use it even if I read the explanation. I would like you to explain how to use from 1 in movies.
This review is about item#08756167.
Work related to interior work
1
From Japan
On 2009-03-06 08:47:00
I think that this product is a durable low price sharpener on a do-it-yourself level, but I think it is difficult if it is difficult to match the angle and it is difficult to match the angle although the drill is reversed, but I think that it is difficult Because it is low, it is best to use it only at disposable level.
This review is about item#08756167.
Drill polishing
1
From Japan
On 2008-12-12 17:06:40
It is not usable at all. Is there anyone who can master this?
This review is about item#08756167.
One polished to try a 4.2 mm iron drill polished with a grinder.
1
From Japan
On 2008-08-07 23:01:47
The angle of the cutting edge gradually became obtuse angle before I could not polish one of them. When I tried disassembling the sharpener, the grinding stone was wearing stepped and no more angle. It became inoperable before polishing even one. The grindstone is too soft.
This review is about item#08756167.
1
Customer Who Viewed This Item Also Viewed
ATMA WHEEL Φ 100 NO AXIS
Drill Sharpener
2.4-13mm, Drill Sharpener
Drill Sharpener, Dori Ken DX
Drill Sha Puna
Diamond Blade Grinder
Drill Sharpener, Dori Ken X A+B Chuck
Doriken X thinning A chuck
Drill Bit Sharpener
2.4-13mm, Drill Sharpener
Drill Bit For Iron Drill