Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Eye Bottle

Eye Bottle
Sales Price: 8.99 SGD
Review Rating: 4.60
5 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Paint thinner.
4
From Japan
On 2018-02-10 00:16:01
The bottle that I used to divide was always broken and I bought it instead. At the top marked (2/3 place of the bottle) is 500 ml, and if you put the lid all the way, it will enter 700 ml. I would like to mention the maximum capacity ....
This review is about item#09155203.
It is used for storing chemicals.
5
From Japan
On 2018-01-04 16:45:28
The size of the mouth is just right, making it sturdier than anything is good.
This review is about item#9155237.
Chemical storage
5
From Japan
On 2017-11-14 22:14:31
It does not break even if it bumps somewhat with a tough bottle. It is convenient to carry and it is a transparent bottle so it was easy to check the liquid.
This review is about item#9155176.
Storage of chemicals
4
From Japan
On 2015-10-26 15:03:44
The main body glass, the lid can be made firmly, but packing of the lid is somewhat difficult. Just by turning the lid upside down it falls with a porridge. When working on a desk it is necessary to pay attention to where to place the lid. If you adjust the lid when you tighten up, packing will fall off somewhat. Well there are also good things because you can wash well packing up with that. I do not yet know the sealability. Since the trace of the bottle mouth is clearly attached to the packing, it seems that it is closed as it is.
This review is about item#09155237.
Storage of organic solvents and aqueous solutions
5
From Japan
On 2015-02-11 17:38:59
I use it to temporarily preserve organic solvents and aqueous solutions. This product is a pair of glass bottle part, plastic cap part and inner solvent resistant packing part. If you use it for a long time, the cap may crack or the packing may become dirty so it is saved to purchase additional parts separately. It is even better if there is an optional part only for the glass part.
This review is about item#09155203.
1