Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Rain Overalls

Rain Overalls
Sales Price: 59.99 SGD
Review Rating: 4.12
8 Customer Reviews
5 star 3
4 star 3
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
When working outdoors rainy weather
From Japan
On 2017-07-30 23:01:08
The fabric is solid and highly waterproof. It is also nice not to get in the way when not in use because it can store the hood. However, because the breathability also falls a bit, the sweat and the inside moisture will eventually end up with a shimmering but it is rain gear that can not be avoided anymore. Since there is no elongation, it is hard to bend and it can not deny the side that is difficult to move. If it is separate upper and lower, rain may leak from the waist when bending, but it is enough that it does not exist.
Livestock sampling
From Japan
On 2016-07-12 16:13:28
I am glad that it is not hot because the inside is a mesh.
This review is about item#09157066.
Pesticide spraying
From Japan
On 2015-09-18 19:45:37
I use it when spraying pesticides. I wear this tether, I am wearing goggles and masks on it. 176 cm, standard body type LL was exactly right. Although it has only a mesh, it is hard in the midsummer as it was in the sauna condition.
This review is about item#09157057.
Used outside work
From Japan
On 2015-01-09 10:09:20
I think that it is even better if there are color variations
This review is about item#09157057.
Measures on rainy days
From Japan
On 2014-09-05 08:12:24
Other people pointed out, but it is not suitable for riding a motorcycle. Other than that, I like it both functionally and stylistically.
This review is about item#09157057.
When moving on a motorcycle
From Japan
On 2013-10-15 22:29:35
This product is well made and well made. It is not fluffy, not thick, moderate thickness, the back is mesh and easy to remove. Waterproofing is quite good so it will be very good for working outside. However, when used in a motorcycle (125 cc scooter) water will invade from the bottom of the zipper. Structurally, when sitting down due to front bending, dripping drips Since rain invades the crotch, it is not suitable for use as a motorcycle.
This review is about item#09157127.
for work
From Japan
On 2011-11-25 12:44:46
It is unexpectedly firm making. The article is not that thin, and this is the best thing. In addition, because it is an tsunagi type, there is no tightening with the rubber of the trousers like an ordinary two piece, so "Mure" will not get wet with your own sweat. When the hood is unnecessary, it can be rolled and stored in the collar part. If this color, dirt is not noticeable and warm, so you can use it as a warm clothes. I personally think that it is cuckoo.
This review is about item#09157032.
In the shipping industry
From Japan
On 2011-11-19 12:32:46
I think that the size up a notch is better than my size.
This review is about item#09157102.
Customer Who Viewed This Item Also Viewed
Rainwear, Pegasus
Rain Alpha
Rain Strong Alpha, Camouflage
Raincoat Work
Starting Pack
Safety Rain Suit