Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Magic type sandpaper HNAR type roll (100-mm width)

Magic type sandpaper HNAR type roll (100-mm width)
Sales Price: 65.99 SGD
Review Rating: 4.17
6 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
I polish it by cutting it to the necessary length for polishing machines, rotating it and polishing it.
2
From Japan
On 2017-09-29 15:24:06
Whether it was not enough for the length of the regulation or another meaning, I added a few meters with tape. It cuts it to the necessary length and it is used, so if it is supplemented on the way, it makes me feel a little lost.
This review is about item#8726636.
Process after welding
4
From Japan
On 2017-09-19 00:27:22
It is very convenient because it can easily be cut to the size you like, but I think that I am thankful that there will be a little more strength as it will do as it is, so it will last longer.
This review is about item#08726611.
Kindergarten wooden floor paint used for Linax Porche
5
From Japan
On 2016-01-17 07:05:02
Because genuine paper is expensive, I used it by cutting it, but it was able to be used without problems. Shipment was also early and it was saved.
This review is about item#08726602.
Polishing of putty
5
From Japan
On 2014-06-19 20:14:22
Is the abrasive different? Even if it is lighter than the product we used until now, the effect is the same, durability is good and it is excellent in cost. It is usually economical to cut the width by 75 mm width and divert the rest.
This review is about item#08726611.
Removal of flaws such as machine rolls
4
From Japan
On 2008-11-20 15:49:56
It is even better if it is easy to cut paper with good water resistance and abrasiveness
This review is about item#08726611.
Scratch and rust removal of die set · machine etc.
5
From Japan
On 2008-05-21 12:40:47
It is easy to use with cutout type, and it is profitable because there is 15 m.
This review is about item#08726611.
1
Customer Who Viewed This Item Also Viewed
Sanding Paper,
Magic type sandpaper HNAR  roll (75-mm width)
Stikit Gold Finishing  Roll
PPS N
  • PPS N
  • FUJI STAR (Sankyo-Rikagaku)
  • 67.99 SGD
Sandpaper Rolls
Autonet roll (100 x 10m)
Sanding Roll 75x10m
Pop-up roll paper
Magic tuck roll (115mm width)
Dry Paper Disc, 75mm Width
Dry Paper Disc
PS Paper R